This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:eval-adxrs290-pmdz [09 Mar 2022 21:01] – fix link Robin Getz | resources:eval:user-guides:circuits-from-the-lab:eval-adxrs290-pmdz [27 Jan 2023 09:23] – Replaced the obsolete Kuiper Linux page link Joyce Velasco | ||
---|---|---|---|
Line 144: | Line 144: | ||
* **Software** | * **Software** | ||
- | * [[: | + | * [[: |
==== Loading Image on SD Card ==== | ==== Loading Image on SD Card ==== | ||
- | In order to control the **EVAL-ADXRS290-PMDZ** from the Raspberry Pi, you will need to install ADI Kuiper Linux on an SD card. Complete instructions, | + | In order to control the **EVAL-ADXRS290-PMDZ** from the Raspberry Pi, you will need to install ADI Kuiper Linux on an SD card. Complete instructions, |
\\ | \\ | ||
Write the image and follow the system configuration procedure. | Write the image and follow the system configuration procedure. | ||
==== Configuring the SD Card ==== | ==== Configuring the SD Card ==== | ||
- | Follow the Hardware Configuration procedure under **Preparing the Image: Raspberry Pi** in the [[: | + | Follow the Hardware Configuration procedure under **Preparing the Image: Raspberry Pi** in the [[: |
< | < | ||
Line 326: | Line 326: | ||
* [[https:// | * [[https:// | ||
* [[https:// | * [[https:// | ||
- | * [[: | + | * [[: |
=====Registration===== | =====Registration===== |