Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:circuits-from-the-lab:cn0566 [25 Sep 2022 16:59] – Update tapering video Mark Thoren | resources:eval:user-guides:circuits-from-the-lab:cn0566 [15 Jun 2023 20:52] (current) – [Phased Array Software] Dongmin Lee |
---|
====== Phaser Landing Page ====== | ====== CN0566 Phased Array User Guide ====== |
Note: This page and Phaser release are still in development, but hitting some delays. Please check back soon for more updates and product release information. | |
\\ | |
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0566:phasers_to_fun.png?direct&800 |}} | |
\\ | |
===== Introduction: ===== | |
Phased array communications and radar systems are finding increased use in a variety of applications. This places a greater importance on training engineers and rapidly prototyping new phased array concepts. However, both those imperatives have historically been difficult and expensive. That is why Analog Devices is (soon!) launching the ADALM-PHASER. It is a low cost, simplified phased array radar which allows real beamforming hardware to be used for education, project proposals, and even software development. | |
| |
Here is a brief video introduction to the phaser: | ===== Introduction ===== |
{{youtube>dUn2_fiOh94}} | |
| Phased array communications and radar systems are finding increased use in a variety of applications. This places a greater importance on training engineers and rapidly prototyping new phased array concepts. However, both those imperatives have historically been difficult and expensive. That is why Analog Devices launched the ADALM-PHASER. It is a low cost, simplified phased array radar which allows real beamforming hardware to be used for education, project proposals, and even software development.\\ |
| Most of the labs are run on a Python GUI, with several helper scripts. These can be run on a remote host computer, or directly on the phaser's Raspberry Pi computer with the addition of a keyboard, mouse, and display.\\ |
| For more advanced application development, the Phaser is also supported in the MATLAB RF Microwave Toolbox. Equivalent MATLAB lab exercises are in development, and will be added below as they are completed. |
| |
===== Phaser Hardware ===== | |
* When??? We’re hitting some delays due to part availability. But we hope to have ordering information available by end of July 2022. | |
* To get acquainted with the hardware, see the **[[resources:eval:user-guides:circuits-from-the-lab:cn0566:overview_setup|Phaser Hardware Overview]]** page. | |
\\ | |
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0566:phaser_with_topics.png?600 |}} | {{ :resources:eval:user-guides:circuits-from-the-lab:cn0566:phaser_with_topics.png?600 |}} |
| |
| Here is a brief video introduction to beamforming and the Phased Array Platform: |
| <WRAP centeralign> |
| {{youtube>dUn2_fiOh94?large}} |
| </WRAP> |
| |
| ===== Quick Start Guide ===== |
| * There are a few steps that need to be performed before diving into the lab exercises. Please visit the **[[:resources:eval:user-guides:circuits-from-the-lab:cn0566:quickstart|Quick Start Guide]]**. |
\\ | \\ |
| ===== Phased Array Hardware ===== |
| |
| * To get acquainted with the hardware, see the **[[resources:eval:user-guides:circuits-from-the-lab:cn0566:overview_setup|Phaser Hardware Overview]]** page. |
| |
| ===== Phased Array Software ====== |
| |
| There are several pieces of software used with the CN0566 Phaser, including a user-friendly Graphical User Interface (GUI) and a number of command-line utilities. This page describes the various pieces of software: |
| |
| * **[[resources:eval:user-guides:circuits-from-the-lab:cn0566:software|Phaser Software guides (GUI and CLI utilities)]]** |
| * **[[:phaser_matlab|Phaser Software guide for MATLAB]]** |
| ===== Phased Array Assembly and Testing ====== |
| |
| The phaser ships fully assembled and ready to go. Should you need to re-assemble a disassembled board, or do a quick functionality test, refer to this page: |
| |
| * **[[resources:eval:user-guides:circuits-from-the-lab:cn0566:assy_prod_test|CN0566 Assembly and Production Test]]** |
| |
===== Labs and Lectures ===== | ===== Labs and Lectures ===== |
| |
| {{ :resources:eval:user-guides:circuits-from-the-lab:cn0566:phasers_to_fun.png?direct&800 |}} |
| |
The ADALM-PHASER is meant for you to experience, first hand, phased array beamforming and radar concepts. But to go along with the hardware, we’ve put together a series of short lectures followed by hands-on labs that you can perform with your own Phaser. A complete, printable lab manual is available here: | The ADALM-PHASER is meant for you to experience, first hand, phased array beamforming and radar concepts. But to go along with the hardware, we’ve put together a series of short lectures followed by hands-on labs that you can perform with your own Phaser. A complete, printable lab manual is available here: |
<WRAP round 80% download> | <WRAP round 80% download> |
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0566:phaser_lab_instructions_june14_2022_no_title.docx |Printable Phaser Lab Instructions (DOCX)}} | **{{ :resources:eval:user-guides:circuits-from-the-lab:cn0566:phaser_lab_instructions_june14_2022_no_title.docx |Printable Phaser Lab Instructions (DOCX)}}** |
\\ | |
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0566:phaser_lab_instructions_june14_2022_no_title.pdf |Printable Phaser Lab Instructions (PDF)}} | **{{ :resources:eval:user-guides:circuits-from-the-lab:cn0566:phaser_lab_instructions_june14_2022_no_title.pdf |Printable Phaser Lab Instructions (PDF)}}** |
</WRAP> | </WRAP> |
\\ | |
The expanded list of topics is as follows: | The expanded list of topics is as follows: |
| |
* Phaser Hardware Overview and Frequency Plan | * Phaser Hardware Overview, Software Setup, and Frequency Plan |
* **[[resources:eval:user-guides:circuits-from-the-lab:cn0566:overview_setup|Schematics, Layout and Operation]]** | * **[[resources:eval:user-guides:circuits-from-the-lab:cn0566:overview_setup|Phaser Hardware Overview]]** |
* Lecture Video | * Lecture Video |
* {{youtube>-Vqbgf0MjPk?small}} | * {{youtube>-Vqbgf0MjPk?small}} |
| |
* Basics of SDR and Beamforming Control | * Basics of SDR and Beamforming Control |
* **[[resources:eval:user-guides:circuits-from-the-lab:cn0566:calibration|Lab Material]]** | * **[[resources:eval:user-guides:circuits-from-the-lab:cn0566:basic_example|Lab: Controlling the Phaser with Python]]** |
| * **[[resources:eval:user-guides:circuits-from-the-lab:cn0566:matlab_basic_example|Lab: Controlling the Phaser with MATLAB]]** |
* Lecture Video | * Lecture Video |
* {{youtube>jBGzOlThpRE?small}} | * {{youtube>jBGzOlThpRE?small}} |
* Grating Lobes | * Grating Lobes |
* **[[resources:eval:user-guides:circuits-from-the-lab:cn0566:grating_lobes|Lab Material]]** | * **[[resources:eval:user-guides:circuits-from-the-lab:cn0566:grating_lobes|Lab Material]]** |
* Lecture Video (Coming Soon) | * Lecture and Lab Video |
* Lab Video (Coming Soon) | * {{youtube>qksh4lGysbI?small}} |
| |
* Beam Squint | * Beam Squint |
* **[[resources:eval:user-guides:circuits-from-the-lab:cn0566:beam_squint|Lab Material]]** | * **[[resources:eval:user-guides:circuits-from-the-lab:cn0566:beam_squint|Lab Material]]** |
* Lecture Video (Coming Soon) | * Lecture and Lab Video |
* Lab Video (Coming Soon) | * {{youtube>LYVD014ClZI?small}} |
| |
* Quantization Sidelobes | * Quantization Sidelobes |
* **[[resources:eval:user-guides:circuits-from-the-lab:cn0566:quantization_sidelobes|Lab Material]]** | * **[[resources:eval:user-guides:circuits-from-the-lab:cn0566:quantization_sidelobes|Lab Material]]** |
* Lecture Video (Coming Soon) | * Lecture and Lab Video |
* Lab Video (Coming Soon) | * {{youtube>51O5FLVZE4c?small}} |
| |
* Analog, Digital, and Hybrid Beamforming | * Analog, Digital, and Hybrid Beamforming |
* **[[resources:eval:user-guides:circuits-from-the-lab:cn0566:hybrid_beamforming|Lab Material]]** | * **[[resources:eval:user-guides:circuits-from-the-lab:cn0566:hybrid_beamforming|Lab Material]]** |
* Lecture Video (Coming Soon) | * Lecture and Lab Video |
* Lab Video (Coming Soon) | * {{youtube>hMiJs2NdXZY?small}} |
| |
* Monopulse Tracking | * Monopulse Tracking |
* **[[resources:eval:user-guides:circuits-from-the-lab:cn0566:monopulse_tracking|Lab Material]]** | * **[[resources:eval:user-guides:circuits-from-the-lab:cn0566:monopulse_tracking|Lab Material]]** |
* Lecture Video (Coming Soon) | * Lecture and Lab Video |
* Lab Video (Coming Soon) | * {{youtube>hZDopcNjVzY?small}} |
| |
* Radar: Simple FMCW | * Radar: Simple FMCW |
* **[[resources:eval:user-guides:circuits-from-the-lab:cn0566:fmcw_radar|Lab Material]]** | * **[[resources:eval:user-guides:circuits-from-the-lab:cn0566:fmcw_radar|Lab Material]]** |
* Lecture Video (Coming Soon) | * Lecture and Lab Video |
* Lab Video (Coming Soon) | * {{youtube>CXSbLQgRFAA?small}} |
| |
* Radar: CFAR, Range Normalization, Clutter Suppression, and Range/Velocity | * Radar: CFAR, Range Normalization, Clutter Suppression, and Range/Velocity |
| |
| |
===== Resources ===== | ===== Additional Resources ===== |
| |
This series is partially derived from several sources that also provide valuable background information. | This series is partially derived from several sources that also provide valuable background information. |
* ToDo: Link to Webinar seminars and labs | |
* Analogue Dialogue Phased array paper series: | * Analogue Dialogue Phased array paper series: |
* [[adi>en/analog-dialogue/articles/phased-array-antenna-patterns-part1.html|Phased Array Antenna Patterns—Part 1: Linear Array Beam Characteristics and Array Factor]] | * [[adi>en/analog-dialogue/articles/phased-array-antenna-patterns-part1.html|Phased Array Antenna Patterns—Part 1: Linear Array Beam Characteristics and Array Factor]] |
* [[adi>en/analog-dialogue/articles/phased-array-antenna-patterns-part2.html|Phased Array Antenna Patterns—Part 2: Grating Lobes and Beam Squint]] | * [[adi>en/analog-dialogue/articles/phased-array-antenna-patterns-part2.html|Phased Array Antenna Patterns—Part 2: Grating Lobes and Beam Squint]] |
* [[adi>en/analog-dialogue/articles/phased-array-antenna-patterns-part3.html|Phased Array Antenna Patterns—Part 3: Sidelobes and Tapering]] | * [[adi>en/analog-dialogue/articles/phased-array-antenna-patterns-part3.html|Phased Array Antenna Patterns—Part 3: Sidelobes and Tapering]] |
* 2020 GNURadio workship on Phased Arrays: | |
* **[[https://github.com/jonkraft/PhasedArray/blob/master/PhasedArrayWorkshop_Presentation.pdf|GRCon Phased Array Workshop Slides]]** | |
{{youtube>0hnWfTvETcU?medium}} | |
| |
| ===== More Information and Useful Links ===== |
| * [[ADI>CN0566|CN0566 Product Page]] |
===== Other Resources ====== | * [[:resources:eval:user-guides:circuits-from-the-lab:cn0566:software | CN0566 Software Guide]] |
* **[[resources:eval:user-guides:circuits-from-the-lab:cn0566:software|Phaser Software guides (GUI and CLI utilities)]]** | * [[:resources:eval:user-guides:circuits-from-the-lab:cn0566:overview_setup | CN0566 Hardware Guide]] |
* **[[resources:eval:user-guides:circuits-from-the-lab:cn0566:assy_prod_test|CN0566 Assembly and Production Test]]** | |
| |
//End of Document// | //End of Document// |