This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:circuits-from-the-lab:cn0566:software [08 Apr 2022 01:32] – Update figures, more GUI details Mark Thoren | resources:eval:user-guides:circuits-from-the-lab:cn0566:software [08 Apr 2022 01:34] (current) – [GUI operation] add calibration command Mark Thoren | ||
---|---|---|---|
Line 22: | Line 22: | ||
python3 cn0566_gui.py | python3 cn0566_gui.py | ||
</ | </ | ||
- | which will print debug information to the console as shown below. In this case, gain and phase calibration files were not present, but a frequency measurement file for an HB100 was found. | + | which will print debug information to the console as shown below. In this case, gain and phase calibration files were not present, but a frequency measurement file for an HB100 was found.\\ |
+ | **Typical console output:** | ||
< | < | ||
analog@phaser: | analog@phaser: | ||
Line 46: | Line 47: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
- | Close the GUI, Run the calibration routine to generate calibration files, then re-start. The beam should be much closer to ideal, with first side lobes approximately 13dB below the main lobe. | + | Close the GUI, Run the calibration routine to generate calibration files: |
+ | < | ||
+ | python3 cn0566_examples.py cal | ||
+ | </ | ||
+ | Then re-start | ||
{{ : | {{ : |