This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0566:quickstart [25 May 2023 01:39] – Update video Mark Thoren | resources:eval:user-guides:circuits-from-the-lab:cn0566:quickstart [06 Jul 2023 01:37] – Add HB100 step file Mark Thoren | ||
---|---|---|---|
Line 36: | Line 36: | ||
* Wired or Wireless network connection, with access to the internet (for accessing update files from Github.) | * Wired or Wireless network connection, with access to the internet (for accessing update files from Github.) | ||
\\ | \\ | ||
+ | <WRAP lo round download 80%> | ||
+ | This is the step file for the HB100 holder, with a 1/4-20 thread for a standard camera mount. HB100s can vary from manufacturer to manufacturer, | ||
+ | \\ | ||
+ | Alternatively, | ||
+ | \\ | ||
+ | **{{ : | ||
+ | </ | ||
---- | ---- | ||