This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0566:quickstart [29 Apr 2023 00:03] – More cleanup. Mark Thoren | resources:eval:user-guides:circuits-from-the-lab:cn0566:quickstart [06 Jul 2023 01:37] – Add HB100 step file Mark Thoren | ||
---|---|---|---|
Line 7: | Line 7: | ||
- | ===== Videos | + | ===== Unboxing / Setup Video ===== |
<WRAP centeralign> | <WRAP centeralign> | ||
- | {{youtube> | + | {{youtube> |
- | \\ | + | |
- | **(The Phaser comes mostly assembled. Start at around 12:45, after it's been completely assembled.) ** | + | |
</ | </ | ||
Line 38: | Line 36: | ||
* Wired or Wireless network connection, with access to the internet (for accessing update files from Github.) | * Wired or Wireless network connection, with access to the internet (for accessing update files from Github.) | ||
\\ | \\ | ||
+ | <WRAP lo round download 80%> | ||
+ | This is the step file for the HB100 holder, with a 1/4-20 thread for a standard camera mount. HB100s can vary from manufacturer to manufacturer, | ||
+ | \\ | ||
+ | Alternatively, | ||
+ | \\ | ||
+ | **{{ : | ||
+ | </ | ||
---- | ---- | ||