This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:circuits-from-the-lab:cn0560 [14 Jun 2022 01:10] – [Hardware Description] Rainier Rosario | resources:eval:user-guides:circuits-from-the-lab:cn0560 [14 Jun 2022 01:24] (current) – [Navigating the Evaluation Software] Rainier Rosario | ||
---|---|---|---|
Line 191: | Line 191: | ||
==== Navigating the Evaluation Software ==== | ==== Navigating the Evaluation Software ==== | ||
- | Upon opening ACE, the ADAQ23878 Board should be detected as shown on Figure 17. | + | Upon opening ACE, the ADAQ23878 Board should be detected as shown in Figure 17. |
\\ | \\ | ||
\\ | \\ | ||
Line 199: | Line 199: | ||
\\ | \\ | ||
\\ | \\ | ||
- | From the Main Window, double click on the ADAQ23878 board to open the Board View as shown on Figure 18. | + | From the Main Window, double click on the ADAQ23878 board to open the Board View as shown in Figure 18. |
\\ | \\ | ||
\\ | \\ | ||
Line 208: | Line 208: | ||
{{ : | {{ : | ||
\\ | \\ | ||
- | From Board View, double click on the ADAQ23878 icon to open the Chip View as shown on Figure 19. | + | From Board View, double click on the ADAQ23878 icon to open the Chip View as shown in Figure 19. |
\\ | \\ | ||
\\ | \\ | ||
Line 226: | Line 226: | ||
* Capture Panel | * Capture Panel | ||
\\ | \\ | ||
- | Throughputs. The default throughput (sampling frequency) is 15MSPS. The user can adjust | + | Throughput. The default throughput (sampling frequency) is 15MSPS. The user can adjust throughput to a minimum of 20 kSPS. If the user enters a value larger than ability of the existing device, the software reverts to the maximum throughput. Refer to the ADAQ23878/ |
\\ | \\ | ||
The Number of samples dropdown list in the Capture Settings section allows the user to select the number of samples per channel per capture. The maximum number of samples the software can support is 1048576. | The Number of samples dropdown list in the Capture Settings section allows the user to select the number of samples per channel per capture. The maximum number of samples the software can support is 1048576. | ||
Line 232: | Line 232: | ||
Device Setting Digital Input that Enables Two-Lane Output Mode and One lane mode. When TWOLANES is connected high (two-lane output mode), the [[adi> | Device Setting Digital Input that Enables Two-Lane Output Mode and One lane mode. When TWOLANES is connected high (two-lane output mode), the [[adi> | ||
\\ | \\ | ||
- | Software Oversampling Ratio box as shown in Figure 13 sets the oversampling ratio applied to the captured data. After this control is set to any value other than " | + | Software Oversampling Ratio box as shown in Figure 13 sets the oversampling ratio applied to the captured data. Oversampling refers to sampling faster than twice the signal bandwidth required for Nyquist criterion. |
\\ | \\ | ||
\\ | \\ | ||
Line 239: | Line 239: | ||
The General Settings section allows the user to set up the preferred configuration of the FFT analysis. This configuration sets how many tones are analyzed and if the fundamental is set manually. | The General Settings section allows the user to set up the preferred configuration of the FFT analysis. This configuration sets how many tones are analyzed and if the fundamental is set manually. | ||
\\ | \\ | ||
- | The Windowing section allows the user to set up the preferred windowing type to use in the FFT analysis and the number of harmonic bins and fundamental bins that must be included in the analysis. | + | The Windowing section allows the user to set up preferred windowing type to use in the FFT analysis and the number of harmonic bins and fundamental bins that must be included in the analysis. |
\\ | \\ | ||
- | The Single Tone Analysis and the Two-Tone Analysis sections | + | The Single Tone Analysis and the Two-Tone Analysis sections |
\\ | \\ | ||
\\ | \\ | ||
Line 297: | Line 297: | ||
The INL and DNL tab displays linearity analysis. INL is the deviation of each individual code from a line drawn from negative full scale through positive full scale. The point used as negative full scale occurs ½ LSB before the first code transition. Positive full scale is defined as a level 1½ LSB beyond the last code transition. The deviation is measured from the middle of each code to the true straight line. | The INL and DNL tab displays linearity analysis. INL is the deviation of each individual code from a line drawn from negative full scale through positive full scale. The point used as negative full scale occurs ½ LSB before the first code transition. Positive full scale is defined as a level 1½ LSB beyond the last code transition. The deviation is measured from the middle of each code to the true straight line. | ||
\\ | \\ | ||
- | In an ideal ADC, code transitions are 1 LSB apart. DNL is the maximum deviation from this ideal value. DNL is often specified in terms of resolution for which no missing codes are guaranteed. | + | In an ideal μModule, code transitions are 1 LSB apart. DNL is the maximum deviation from this ideal value. DNL is often specified in terms of resolution for which no missing codes are guaranteed. |
\\ | \\ | ||
To perform a linearity test, apply a sinusoidal signal with 0.5 dB above full scale to the EVAL-CN0560-FMCZ board at the VIN+ and VIN− Subminiature Version A (SMA) inputs. Set the number of hits per code and adjust to the desired accuracy. Using a large number of hits per code results in a significant test time. The figures above display captured data that includes the ±INL and ±DNL positions. | To perform a linearity test, apply a sinusoidal signal with 0.5 dB above full scale to the EVAL-CN0560-FMCZ board at the VIN+ and VIN− Subminiature Version A (SMA) inputs. Set the number of hits per code and adjust to the desired accuracy. Using a large number of hits per code results in a significant test time. The figures above display captured data that includes the ±INL and ±DNL positions. |