This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0554 [12 Dec 2022 02:35] – Joyce Velasco | resources:eval:user-guides:circuits-from-the-lab:cn0554 [27 Jan 2023 09:19] – Replaced the obsolete Kuiper Linux page link Joyce Velasco | ||
---|---|---|---|
Line 18: | Line 18: | ||
* USB keyboard and mouse | * USB keyboard and mouse | ||
* **Software** | * **Software** | ||
- | * [[: | + | * [[: |
===== Connectors and Jumper Configurations ===== | ===== Connectors and Jumper Configurations ===== | ||
Line 54: | Line 54: | ||
^ Main power setup | ^ Main power setup | ||
| {{ : | | {{ : | ||
- | |||
- | ===== Dither and Toggle Controls ===== | ||
- | \\ | ||
- | \\ | ||
- | \\ | ||
===== System Setup ===== | ===== System Setup ===== | ||
Line 76: | Line 71: | ||
* Digital voltmeter (6-digit or higher) | * Digital voltmeter (6-digit or higher) | ||
**Software** | **Software** | ||
- | * [[: | + | * [[: |
**Documentation** | **Documentation** | ||
* [[adi> | * [[adi> | ||
Line 108: | Line 103: | ||
==== Downloading and Flashing Kuiper Linux Image on SD Card ==== | ==== Downloading and Flashing Kuiper Linux Image on SD Card ==== | ||
- | In order to control the **EVAL-CN0554-RPIZ** from the Raspberry Pi, you will need to install ADI Kuiper Linux on an SD card. Complete instructions, | + | In order to control the **EVAL-CN0554-RPIZ** from the Raspberry Pi, you will need to install ADI Kuiper Linux on an SD card. Complete instructions, |
{{ : | {{ : | ||
Line 116: | Line 111: | ||
For the Linux kernel to identify the device connected to the expansion header, update the device tree overlay. A **Device Tree Overlay** contains information about additional connected hardware, the EVAL-CN0554-RPIZ for this case. The overlay file is already included in the SD card and just needs to be matched to the EVAL-CN0554-RPIZ. | For the Linux kernel to identify the device connected to the expansion header, update the device tree overlay. A **Device Tree Overlay** contains information about additional connected hardware, the EVAL-CN0554-RPIZ for this case. The overlay file is already included in the SD card and just needs to be matched to the EVAL-CN0554-RPIZ. | ||
- | Follow the Hardware Configuration procedure under **Preparing the Image: Raspberry Pi** in the [[: | + | Follow the Hardware Configuration procedure under **Preparing the Image: Raspberry Pi** in the [[: |
This brings up the file in the terminal. Scroll down until the line that begins with " | This brings up the file in the terminal. Scroll down until the line that begins with " | ||
Line 227: | Line 222: | ||
- Run the example script using the command. | - Run the example script using the command. | ||
< | < | ||
+ | |||
+ | <WRAP center round todo 80%> | ||
+ | **Update image, file name, and location** | ||
{{ : | {{ : | ||
+ | |||
+ | |||
<WRAP round 80% download> | <WRAP round 80% download> | ||
Github link for the python sample script: | Github link for the python sample script: | ||
[[https:// | [[https:// | ||
</ | </ | ||
+ | </ | ||
===== Schematic, PCB Layout, Bill of Materials ===== | ===== Schematic, PCB Layout, Bill of Materials ===== | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
Line 251: | Line 251: | ||
* [[: | * [[: | ||
* [[: | * [[: | ||
- | * [[: | + | * [[: |
===== Hardware Registration ===== | ===== Hardware Registration ===== |