This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0548 [22 Sep 2021 03:36] – [Simplified Block Diagram] erbe reyta | resources:eval:user-guides:circuits-from-the-lab:cn0548 [29 Sep 2021 05:49] – [Simplified Block Diagram] erbe reyta | ||
---|---|---|---|
Line 17: | Line 17: | ||
- | | + | |
+ | 1. Place the shunt jumpers connected to P15 as the default position for the Chip Select. | ||
+ | {{ : | ||
+ | 2. Follow the figure below for the position of shunt jumpers for headers P1, P3, P10, P8, P9, and P11. Make sure that is set at 16V max input for the voltage sensing, follow jumper settings stated in the table below encircled in red for 16V maximum input. | ||
{{: | {{: | ||
Line 23: | Line 26: | ||
{{: | {{: | ||
- | 2. Place all the shunt jumpers connected to GND, headers P12, P13, P14 and P7 as default position for measurements in unipolar mode. Refer to the figure below for correct jumper settings. | + | 3. Place all the shunt jumpers connected to GND, headers P12, P13, P14 and P7 as default position for measurements in unipolar mode. Refer to the figure below for correct jumper settings. |
{{ : | {{ : | ||
- | 3. Place the shunt jumpers connected to P15 as the default position for the Chip Select. | + | 4. Place the shunt jumpers connected to P15 as the default position for the Chip Select. |
{{ : | {{ : | ||
- | 4. Referring to step 1, where you uploaded the .hex file firmware to ADICUP3029. Now run the executable GUI “ad7799_py_new.exe” located inside “ad7799_app” folder. It will take for about a minute before the CN0548 app will show up on your PC display. Please see figure 6 for CN0548 GUI upon start. Once the application is running, determine the comport at your device manager window and type it in the “COMPort “ number. See figure below for device manager comport number. Then input the correct comport number then press “connect” button see figure 8 for successful connection. | + | 5. Referring to step 1, where you uploaded the .hex file firmware to ADICUP3029. Now run the executable GUI “ad7799_py_new.exe” located inside “ad7799_app” folder. It will take for about a minute before the CN0548 app will show up on your PC display. Please see figure 6 for CN0548 GUI upon start. Once the application is running, determine the comport at your device manager window and type it in the “COMPort “ number. See figure below for device manager comport number. Then input the correct comport number then press “connect” button see figure 8 for successful connection. |
\\ \\ | \\ \\ |