This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0545 [19 Jul 2022 09:09] – John Carlo Cillion | resources:eval:user-guides:circuits-from-the-lab:cn0545 [05 Sep 2022 08:22] – John Carlo Cillion | ||
---|---|---|---|
Line 45: | Line 45: | ||
* Power the board with a 7 V or 9 V power source connected to J5. | * Power the board with a 7 V or 9 V power source connected to J5. | ||
* Connect the Thermistor and precision reference resistor. See figure below. | * Connect the Thermistor and precision reference resistor. See figure below. | ||
+ | * For Thermistor measurements, | ||
+ | * LK3 - Jumper from REFIN1- to AVSS, this jumper should be inserted. | ||
+ | * LK4 - This jumper is used to apply an external 2.5V or internal 2.5V to REFIN1+, this jumper should be inserted to B. | ||
* Connect the SDP board to the PC via the USB cable. | * Connect the SDP board to the PC via the USB cable. | ||
Line 64: | Line 67: | ||
{{ : | {{ : | ||
==== Demo Mode and ADC Software Configurations ==== | ==== Demo Mode and ADC Software Configurations ==== | ||
- | To configure the [[adi> | + | To configure the [[adi> |
=== Thermistor demo mode === | === Thermistor demo mode === |