This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:circuits-from-the-lab:cn0518 [18 May 2023 17:07] – [Primary Side] making a table Brandon Bushey | resources:eval:user-guides:circuits-from-the-lab:cn0518 [18 May 2023 17:12] (current) – updated some formatting and link styles Brandon Bushey | ||
---|---|---|---|
Line 30: | Line 30: | ||
<wrap center 30%> | <wrap center 30%> | ||
//<fc # | //<fc # | ||
+ | </ | ||
+ | |||
+ | ==== Secondary Side ==== | ||
+ | |||
+ | {{ : | ||
+ | <wrap center 30%> | ||
+ | //<fc # | ||
</ | </ | ||
Line 52: | Line 59: | ||
| ON | ON | Overpower Event (RF Output Attenuated) | | | ON | ON | Overpower Event (RF Output Attenuated) | | ||
- | ==== Secondary Side ==== | + | ==== Power Supply Connector |
- | + | ||
- | {{ : | + | |
- | <wrap center 30%> | + | |
- | //<fc # | + | |
- | </ | + | |
- | + | ||
- | === Power Supply Connector === | + | |
* **P1** is the micro-USB port used to provide 5 V power to the board. | * **P1** is the micro-USB port used to provide 5 V power to the board. | ||
Line 83: | Line 83: | ||
==== ADALM-PLUTO Preparation ==== | ==== ADALM-PLUTO Preparation ==== | ||
Follow the step-by-step process on how to configure the ADALM-PLUTO for proper operation by referring to this [[: | Follow the step-by-step process on how to configure the ADALM-PLUTO for proper operation by referring to this [[: | ||
+ | |||
==== Test Setup ==== | ==== Test Setup ==== | ||
- | === Normal Operation === | + | |
{{ : | {{ : | ||
<wrap center 30%> | <wrap center 30%> | ||
Line 98: | Line 99: | ||
[[: | [[: | ||
</ | </ | ||
- | \\ | + | |
==== IIO Oscilloscope ==== | ==== IIO Oscilloscope ==== | ||
+ | |||
<note important> | <note important> | ||
Line 119: | Line 121: | ||
</ | </ | ||
- | ===== More Information and Useful Links ===== | + | ===== More Information and Useful Links ===== |
* [[ADI> | * [[ADI> | ||
Line 136: | Line 138: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | [[https:// | + | [[adi>CN0518-DesignSupport | EVAL-CN0518-EBZ Design & Integration Files]] |
* Schematics | * Schematics | ||
Line 144: | Line 146: | ||
</ | </ | ||
- | =====Registration===== | + | =====Registration===== |
<WRAP round tip 80% > | <WRAP round tip 80% > | ||
Receive software update notifications and documentation updates, view the latest videos, and more when you register your hardware. | Receive software update notifications and documentation updates, view the latest videos, and more when you register your hardware. | ||
//End of Document// | //End of Document// |