This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0511 [10 Aug 2022 23:01] – updated figure numbers Brandon Bushey | resources:eval:user-guides:circuits-from-the-lab:cn0511 [30 Jan 2023 02:30] – Joyce Velasco | ||
---|---|---|---|
Line 133: | Line 133: | ||
==== Downloading and Flashing Kuiper Linux Image on SD Card ==== | ==== Downloading and Flashing Kuiper Linux Image on SD Card ==== | ||
- | In order to control the **EVAL-CN0511-RPIZ** from the Raspberry Pi, you will need to install ADI Kuiper Linux on an SD card. Complete instructions, | + | In order to control the **EVAL-CN0511-RPIZ** from the Raspberry Pi, you will need to install ADI Kuiper Linux on an SD card. Complete instructions, |
{{ : | {{ : | ||
Line 141: | Line 141: | ||
For the Linux kernel to identify the device connected to the expansion header, update the device tree overlay. A **Device Tree Overlay** contains information about additional connected hardware, the EVAL-CN0511-RPIZ for this case. The overlay file is already included in the SD card and just needs to be matched to the EVAL-CN0511-RPIZ. | For the Linux kernel to identify the device connected to the expansion header, update the device tree overlay. A **Device Tree Overlay** contains information about additional connected hardware, the EVAL-CN0511-RPIZ for this case. The overlay file is already included in the SD card and just needs to be matched to the EVAL-CN0511-RPIZ. | ||
- | Follow the Hardware Configuration procedure under **Preparing the Image: Raspberry Pi** in the [[: | + | Follow the Hardware Configuration procedure under **Preparing the Image: Raspberry Pi** in the [[: |
This brings up the file in the terminal. Scroll down until the line that begins with " | This brings up the file in the terminal. Scroll down until the line that begins with " | ||
Line 266: | Line 266: | ||
=== Running the Example === | === Running the Example === | ||
- | This demo uses a PyADI-IIO example script. | + | This demo uses a PyADI-IIO example script. |
- Connect the [[ADI> | - Connect the [[ADI> | ||
- Open command prompt or terminal and navigate through the examples folder inside the downloaded or cloned // | - Open command prompt or terminal and navigate through the examples folder inside the downloaded or cloned // | ||
Line 294: | Line 294: | ||
* [[: | * [[: | ||
* [[: | * [[: | ||
- | * [[: | + | * [[: |
===== More Information and Useful Links ===== | ===== More Information and Useful Links ===== |