This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0507 [02 Mar 2021 08:04] – Added UART Communication Protocol Jeric Vargas | resources:eval:user-guides:circuits-from-the-lab:cn0507 [30 Jul 2021 07:36] (current) – [Registration] Zuedmar Arceo | ||
---|---|---|---|
Line 79: | Line 79: | ||
- | ===== Porting to other Microcontroller | + | ===== Creating A new PC Applications |
- | This will discuss on how to port the driver and GUI to other microcontroller. | + | This would discuss on how the customers can make their own PC application that could communicate with the existing firmware using UART communication. This also includes the UART settings and communication protocols |
==== UART Configuration ==== | ==== UART Configuration ==== | ||
Line 108: | Line 108: | ||
The table below will show all the available commands with their respective hex code, input values and the return values. | The table below will show all the available commands with their respective hex code, input values and the return values. | ||
{{: | {{: | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | </ | ||
+ | |||
+ | //End of Document// | ||
+ |