This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0507 [07 Jan 2020 08:43] – added calibration tab images Jhake Zebedee Aquino | resources:eval:user-guides:circuits-from-the-lab:cn0507 [14 Jan 2021 05:12] – user interwiki links Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== CN-0507: A Complete 2-Port Network Analyzer on an Arduino Shield ====== | ====== CN-0507: A Complete 2-Port Network Analyzer on an Arduino Shield ====== | ||
This reference design implements a complete 2-Port radio frequency (RF) Network Analyzer using a low-cost zero intermediate frequency (ZIF) architecture in an Arduino form factor, which is designed to plug into EVAL-ADICUP3029. | This reference design implements a complete 2-Port radio frequency (RF) Network Analyzer using a low-cost zero intermediate frequency (ZIF) architecture in an Arduino form factor, which is designed to plug into EVAL-ADICUP3029. | ||
+ | {{ : | ||
---- | ---- | ||
Line 17: | Line 17: | ||
To use the software GUI, the firmware must first be loaded onto the EVAL-ADICUP3029. | To use the software GUI, the firmware must first be loaded onto the EVAL-ADICUP3029. | ||
- Download the hex file from the CN-0507 product page. | - Download the hex file from the CN-0507 product page. | ||
- | - If running an operating system older than Windows 10, install serial driver as in **[[https:// | + | - If running an operating system older than Windows 10, install serial driver as in **[[/ |
- You should see DAPLINK in your list of drives. {{ : | - You should see DAPLINK in your list of drives. {{ : | ||
- Copy the hex file to the DAPLINK drive to load the firmware to the EVAL-ADICUP3029. Note that the DAPLINK drive will disappear for a moment, then reappear after loading the firmware. | - Copy the hex file to the DAPLINK drive to load the firmware to the EVAL-ADICUP3029. Note that the DAPLINK drive will disappear for a moment, then reappear after loading the firmware. |