This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0503:colorimetry [14 Jul 2021 16:40] – updated title Brandon Bushey | resources:eval:user-guides:circuits-from-the-lab:cn0503:colorimetry [14 Jul 2021 16:42] – Brandon Bushey | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Optical Platform: pH Demo ====== | + | ====== Optical Platform: pH Measurement |
Colorimetry can be used to determine the concentration of materials in a solution based on its absorbance. One application of colorimetry is pH measurement with the aid of a coloring reagent. This document details the steps in setting up the EVAL-CN0503-ARDZ for pH measurement. | Colorimetry can be used to determine the concentration of materials in a solution based on its absorbance. One application of colorimetry is pH measurement with the aid of a coloring reagent. This document details the steps in setting up the EVAL-CN0503-ARDZ for pH measurement. |