This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:eval:user-guides:circuits-from-the-lab:cn0428-cn0429-programming-with-custom-firmware [03 Jan 2021 21:55] Robin Getz fix links |
resources:eval:user-guides:circuits-from-the-lab:cn0428-cn0429-programming-with-custom-firmware [14 Jan 2021 05:12] Robin Getz user interwiki links |
||
---|---|---|---|
Line 132: | Line 132: | ||
* Note: this source code is downloaded by the ADuCM355 installer (see below). | * Note: this source code is downloaded by the ADuCM355 installer (see below). | ||
* The project code can now be modified and the Sensor Board can be programmed or debugged according to one of the programming options above. | * The project code can now be modified and the Sensor Board can be programmed or debugged according to one of the programming options above. | ||
- | * Further details of using IAR can be found [[https://wiki.analog.com/resources/eval/user-guides/ev-cog-ad3029lz/tools/iar_guide#ide_setup|here]]. | + | * Further details of using IAR can be found [[/resources/eval/user-guides/ev-cog-ad3029lz/tools/iar_guide#ide_setup|here]]. |
====Downloading and Running the ADuCM355 Installer==== | ====Downloading and Running the ADuCM355 Installer==== |