This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0419 [03 Jan 2021 21:55] – fix links Robin Getz | resources:eval:user-guides:circuits-from-the-lab:cn0419 [05 Jan 2021 16:43] – Updated [[adi>EVAL-CN0419-EBZ|EVAL-CN0419-EBZ]] to [[adi>CN0419|EVAL-CN0419-EBZ]] Ioana Chelaru | ||
---|---|---|---|
Line 15: | Line 15: | ||
===== Required Equipment ===== | ===== Required Equipment ===== | ||
- | * [[adi>EVAL-CN0419-EBZ|EVAL-CN0419-EBZ Evaluation Board]] | + | * [[adi> |
* PC with the following //Minimum Requirements// | * PC with the following //Minimum Requirements// | ||
* PC, Mac, Linux computer, or other host that supports USB | * PC, Mac, Linux computer, or other host that supports USB | ||
Line 34: | Line 34: | ||
==== Speed selection ==== | ==== Speed selection ==== | ||
- | Peripheral devices run at one of three speeds, low (1.5 Mbps), full (12 Mbps), and high (480 Mbps). The [[adi>EVAL-CN0419-EBZ|EVAL-CN0419-EBZ Evaluation Board]] can accommodate the low and full speed operations. Listed below are some examples of peripheral devices for each speed. | + | Peripheral devices run at one of three speeds, low (1.5 Mbps), full (12 Mbps), and high (480 Mbps). The [[adi> |
- Low speed devices | - Low speed devices | ||
* Examples: | * Examples: | ||
Line 55: | Line 55: | ||
{{ : | {{ : | ||
- Set the switch S1 to full speed or low speed operation depending on the peripheral specifications. | - Set the switch S1 to full speed or low speed operation depending on the peripheral specifications. | ||
- | - Connect the peripheral to P2 of the [[adi>EVAL-CN0419-EBZ|EVAL-CN0419-EBZ]] | + | - Connect the peripheral to P2 of the [[adi> |
- | - Plug P1 of the [[adi>EVAL-CN0419-EBZ|EVAL-CN0419-EBZ]] into the USB port of the PC/host | + | - Plug P1 of the [[adi> |
\\ | \\ | ||
==== Running the System ==== | ==== Running the System ==== | ||
- Make sure the setting for S1 is correct based on the peripheral device. | - Make sure the setting for S1 is correct based on the peripheral device. | ||
- | -Plug P1 of the board into the PC/host, the [[adi>EVAL-CN0419-EBZ|EVAL-CN0419-EBZ]] is automatically turned on and providing isolation. DS1 will light up as an indication that the board is delivering power to the peripheral device. | + | -Plug P1 of the board into the PC/host, the [[adi> |
-The PC/host must recognize the peripheral connected to make sure the setup is working. | -The PC/host must recognize the peripheral connected to make sure the setup is working. | ||
-Upon successful connection, you can now provide your peripheral the isolated power! | -Upon successful connection, you can now provide your peripheral the isolated power! |