Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0401 [16 Dec 2019 23:06] – [Power Supply Connections and Configuration] Jason Nasoresources:eval:user-guides:circuits-from-the-lab:cn0401 [06 Feb 2021 21:01] (current) – fix link Robin Getz
Line 13: Line 13:
 ----- -----
  
-The [[ADI>CN0401]] connects to the [[ADI>ADICUP3029]] or any Arduino Uno form-factor development platform using the mating headers. Shown below are the hardware connections and jumper headers which configure the operation of the board. +The [[ADI>CN0401]] connects to the [[ADI>EVAL-ADICUP3029|ADICUP3029]] or any Arduino Uno form-factor development platform using the mating headers. Shown below are the hardware connections and jumper headers which configure the operation of the board. 
  
 {{ :resources:eval:user-guides:circuits-from-the-lab:cn0401:cn0401_silkscreen_-_edited.png?nolink&600 |}} {{ :resources:eval:user-guides:circuits-from-the-lab:cn0401:cn0401_silkscreen_-_edited.png?nolink&600 |}}
Line 30: Line 30:
 **P20 Header Shunt Positions for Setting Board Power Source** **P20 Header Shunt Positions for Setting Board Power Source**
 ^  Position              ^  Location  ^Description                            ^ ^  Position              ^  Location  ^Description                            ^
-|  Across pins 1 and 2    {{ :resources:eval:user-guides:circuits-from-the-lab:cn0401:p20v1.png?nolink&50 |}}  |Board sources the required 5V supply for isolated dc-to-dc converter from the 5V Arduino Uno header pin                 | +|  Shunt pins 1 and 2    {{ :resources:eval:user-guides:circuits-from-the-lab:cn0401:p20v1.png?nolink&50 |}}  |Board sources the required supply for the isolated dc-to-dc converter from the 5V Arduino Uno header pin                 | 
-|  Across pins 2 and 3    {{ :resources:eval:user-guides:circuits-from-the-lab:cn0401:p20v2.png?nolink&50 |}}                                      |Board sources the required 5V supply for the isolated dc-to-dc converter from the External Supply Terminal Block (P6-Pin 1)  |+|  Shunt pins 2 and 3    {{ :resources:eval:user-guides:circuits-from-the-lab:cn0401:p20v2.png?nolink&50 |}}                                      |Board sources the required supply for the isolated dc-to-dc converter from the External Supply Terminal Block (P6-Pin 1)  |
 **P11 Header Shunt Positions for Setting Board Voltage Logic** **P11 Header Shunt Positions for Setting Board Voltage Logic**
 ^  Position              ^  Location  ^Description                               ^ ^  Position              ^  Location  ^Description                               ^
-|  Across pins 1 and 2    {{ :resources:eval:user-guides:circuits-from-the-lab:cn0401:p11v1.png?nolink&50 |}}          |Board sources the logic supply from the IOREF Arduino Uno Header Pin                 | +|  Shunt pins 1 and 2    {{ :resources:eval:user-guides:circuits-from-the-lab:cn0401:p11v1.png?nolink&50 |}}          |Board sources the logic supply from the IOREF Arduino Uno Header Pin                 | 
-|  Across pins 2 and 3    {{ :resources:eval:user-guides:circuits-from-the-lab:cn0401:p11v2.png?nolink&50 |}}          |Board sources the logic supply from the External Supply Terminal Block (P6-Pin 2). The logic levels will scale with the supply voltage and typically must match the level of the development platform.  |+|  Shunt pins 2 and 3    {{ :resources:eval:user-guides:circuits-from-the-lab:cn0401:p11v2.png?nolink&50 |}}          |Board sources the logic supply from the External Supply Terminal Block (P6-Pin 2). The logic levels will scale with the supply voltage and typically must match the level of the development platform.  |
  
 ====CAN Bus Connections==== ====CAN Bus Connections====
Line 64: Line 64:
 **P2 Header Shunt Positions for Setting SPI Chip Select Pin** **P2 Header Shunt Positions for Setting SPI Chip Select Pin**
 ^  Position              ^  Location  ^Description  ^ ^  Position              ^  Location  ^Description  ^
-|  Across pins 1 and 2    {{ :resources:eval:user-guides:circuits-from-the-lab:cn0401:p2v1.png?nolink&100 |}}          |Board uses Arduino pin D10 as chip select          | +|  Shunt pins 1 and 2    {{ :resources:eval:user-guides:circuits-from-the-lab:cn0401:p2v1.png?nolink&100 |}}          |Board uses Arduino pin D10 as chip select          | 
-|  Across pins 3 and 4    {{ :resources:eval:user-guides:circuits-from-the-lab:cn0401:p2v2.png?nolink&100 |}}          |Board uses Arduino pin D9 as chip select           | +|  Shunt pins 3 and 4    {{ :resources:eval:user-guides:circuits-from-the-lab:cn0401:p2v2.png?nolink&100 |}}          |Board uses Arduino pin D9 as chip select           | 
-|  Across pins 5 and 6    {{ :resources:eval:user-guides:circuits-from-the-lab:cn0401:p2v3.png?nolink&100 |}}          |Board uses Arduino pin D8 as chip select           | +|  Shunt pins 5 and 6    {{ :resources:eval:user-guides:circuits-from-the-lab:cn0401:p2v3.png?nolink&100 |}}          |Board uses Arduino pin D8 as chip select           | 
-|  Across pins 7 and 8    {{ :resources:eval:user-guides:circuits-from-the-lab:cn0401:p2v4.png?nolink&100 |}}          |Board uses Arduino pin D7 as chip select           |+|  Shunt pins 7 and 8    {{ :resources:eval:user-guides:circuits-from-the-lab:cn0401:p2v4.png?nolink&100 |}}          |Board uses Arduino pin D7 as chip select           |
  
 ====Silent Mode and Interrupt Configuration==== ====Silent Mode and Interrupt Configuration====
Line 84: Line 84:
 **P19 Shunt Position for Setting Slope Control and Full Speed Mode** **P19 Shunt Position for Setting Slope Control and Full Speed Mode**
 ^  Position              Location  ^Description          ^ ^  Position              Location  ^Description          ^
-|  Across pins 1 and 2  |  {{ :resources:eval:user-guides:circuits-from-the-lab:cn0401:p19v1.png?nolink&50 |}}          |The ADM3055E transceiver is set to full speed mode     | +|  Shunt pins 1 and 2  |  {{ :resources:eval:user-guides:circuits-from-the-lab:cn0401:p19v1.png?nolink&50 |}}          |The ADM3055E transceiver is set to full speed mode     | 
-|  Across pins 2 and 3  |  {{ :resources:eval:user-guides:circuits-from-the-lab:cn0401:p19v2.png?nolink&50 |}}          |The ADM3055E transceiver is set to slope control mode  |+|  Shunt pins 2 and 3  |  {{ :resources:eval:user-guides:circuits-from-the-lab:cn0401:p19v2.png?nolink&50 |}}          |The ADM3055E transceiver is set to slope control mode  |
  
 ====== Software ====== ====== Software ======
-  * [[https://wiki.analog.com/resources/eval/user-guides/eval-adicup3029/reference_designs/demo_cn0401| ADICUP3029 + CN0401 Demo Software and Setup]]+  * [[/resources/eval/user-guides/eval-adicup3029/reference_designs/demo_cn0401| ADICUP3029 + CN0401 Demo Software and Setup]]
  
 ====== Schematic, PCB Layout, Bill of Materials ====== ====== Schematic, PCB Layout, Bill of Materials ======
 <WRAP round 80% download> <WRAP round 80% download>
-[[http://www.analog.com/cn0401-designsupport|CN0401 Design & Integration Files]]+[[adi>cn0401-designsupport|CN0401 Design & Integration Files]]
   * Schematics    * Schematics 
   * PCB Layout    * PCB Layout 
resources/eval/user-guides/circuits-from-the-lab/cn0401.txt · Last modified: 06 Feb 2021 21:01 by Robin Getz