Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:circuits-from-the-lab:cn0393 [23 Mar 2017 18:54] – Tyler Schmitt | resources:eval:user-guides:circuits-from-the-lab:cn0393 [03 Feb 2021 19:33] (current) – Tyler Schmitt |
---|
Digital bank-isolated DAQ designs provide protection for digital backend circuitry and reduce ground loop and common mode interference between banks. They feature multiple DAQ signal chains per ground plane, and can be implemented with fewer digital isolation devices than channel-to-channel isolated systems. | Digital bank-isolated DAQ designs provide protection for digital backend circuitry and reduce ground loop and common mode interference between banks. They feature multiple DAQ signal chains per ground plane, and can be implemented with fewer digital isolation devices than channel-to-channel isolated systems. |
| |
This user guide will discuss how to operate the [[http://www.analog.com/CN0393|EVAL-CN0393-FMCZ]] (CN-0393 Evaluation Hardware), the [[http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/eval-sdp-h1.html|EVAL-SDP-CH1Z]] (SDP-H1) and the [[ftp://ftp.analog.com/pub/cftl/CN0393|CN-0393 Evaluation Software]]. A complete design support package for the CN-0393 evaluation material containing schematics, layouts (native and Gerber), and bill-of-materials can be found at: [[http://www.analog.com/CN0393-DesignSupport|CN0393-DesignSupport]]. | This user guide will discuss how to operate the [[adi>CN0393|EVAL-CN0393-FMCZ]] (CN-0393 Evaluation Hardware), the [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/eval-sdp-h1.html|EVAL-SDP-CH1Z]] (SDP-H1) and the [[ftp://ftp.analog.com/pub/cftl/CN0393|CN-0393 Evaluation Software]]. A complete design support package for the CN-0393 evaluation material containing schematics, layouts (native and Gerber), and bill-of-materials can be found at: [[adi>CN0393-DesignSupport|CN0393-DesignSupport]]. |
| |
| |
===== Required Equipment ===== | ===== Required Equipment ===== |
* [[ADI>CN0393|EVAL-CN0393-FMCZ]] circuit evaluation board | * [[ADI>CN0393|EVAL-CN0393-FMCZ]] circuit evaluation board |
* [[http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/eval-sdp-h1.html|EVAL-SDP-CH1Z]] SDP-H1 controller board | * [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/eval-sdp-h1.html|EVAL-SDP-CH1Z]] SDP-H1 controller board |
* [[ftp://ftp.analog.com/pub/cftl/CN0393|CN-0393 Evaluation Software]] | * [[ftp://ftp.analog.com/pub/cftl/CN0393|CN-0393 Evaluation Software]] |
* +12 V dc switched mode power supply | * +12 V dc switched mode power supply |
| |
===== Getting Started ===== | ===== Getting Started ===== |
The [[ADI>CN0393|EVAL-CN0393-FMCZ]] has a 160-pin FMC connector to interface with a digital host. The SDP-H1 board ([[http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/eval-sdp-h1.html|EVAL-SDP-CH1Z]]) can be used with the [[ftp://ftp.analog.com/pub/cftl/CN0393|CN-0393 Evaluation Software]] to interface with the [[ADI>CN-0393]] hardware (gather conversion results, control gain settings, etc.). It is recommended to install the [[ftp://ftp.analog.com/pub/cftl/CN0393|CN-0393 Evaluation Software]] before connecting/setting up the hardware. See **Installing the CN-0393 Evaluation Software** for instructions for installing the evaluation software and required drivers for the SDP-H1. | The [[ADI>CN0393|EVAL-CN0393-FMCZ]] has a 160-pin FMC connector to interface with a digital host. The SDP-H1 board ([[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/eval-sdp-h1.html|EVAL-SDP-CH1Z]]) can be used with the [[ftp://ftp.analog.com/pub/cftl/CN0393|CN-0393 Evaluation Software]] to interface with the [[ADI>CN0393]] hardware (gather conversion results, control gain settings, etc.). It is recommended to install the [[ftp://ftp.analog.com/pub/cftl/CN0393|CN-0393 Evaluation Software]] before connecting/setting up the hardware. See **Installing the CN-0393 Evaluation Software** for instructions for installing the evaluation software and required drivers for the SDP-H1. |
| |
The [[ADI>CN-0393]] evaluation hardware features an isolation trench that separates two ground planes. When using the hardware (connecting signal generators, scope probes, etc.) be careful that the correct grounds are used and are not connected together. The [[http://www.analog.com/media/en/reference-design-documentation/reference-designs/CN0345.pdf|CN-0393 Circuit Note]] contains detailed information about the hardware. | The [[ADI>CN0393]] evaluation hardware features an isolation trench that separates two ground planes. When using the hardware (connecting signal generators, scope probes, etc.) be careful that the correct grounds are used and are not connected together. The [[adi>media/en/reference-design-documentation/reference-designs/CN0345.pdf|CN-0393 Circuit Note]] contains detailed information about the hardware. |
| |
See **Hardware Setup** for instructions for connecting the [[ADI>CN0393|EVAL-CN0393-FMCZ]] and [[http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/eval-sdp-h1.html|EVAL-SDP-CH1Z]] boards together and to the PC. | See **Hardware Setup** for instructions for connecting the [[ADI>CN0393|EVAL-CN0393-FMCZ]] and [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/eval-sdp-h1.html|EVAL-SDP-CH1Z]] boards together and to the PC. |
| |
===== Installing the CN-0393 Evaluation Software ===== | ===== Installing the CN-0393 Evaluation Software ===== |
===== Hardware Setup ===== | ===== Hardware Setup ===== |
- Before connecting the hardware, install the [[ftp://ftp.analog.com/pub/cftl/CN0393|CN-0393 Evaluation Software]] (see **Installing the CN-0393 Evaluation Software**). | - Before connecting the hardware, install the [[ftp://ftp.analog.com/pub/cftl/CN0393|CN-0393 Evaluation Software]] (see **Installing the CN-0393 Evaluation Software**). |
- Connect P1 on the [[ADI>CN0393|EVAL-CN0393-FMCZ]] board to J4 on the [[http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/eval-sdp-h1.html|EVAL-SDP-CH1Z]] (SDP-H1) board (the 160-pin FMC connector) before applying power. | - Connect P1 on the [[ADI>CN0393|EVAL-CN0393-FMCZ]] board to J4 on the [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/eval-sdp-h1.html|EVAL-SDP-CH1Z]] (SDP-H1) board (the 160-pin FMC connector) before applying power. |
- After connecting the [[ADI>CN0393|EVAL-CN0393-FMCZ]] and [[http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/eval-sdp-h1.html|EVAL-SDP-CH1Z]] boards, connect the +12 V switched mode power supply to the [[http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/eval-sdp-h1.html|EVAL-SDP-CH1Z]] board (via the +12V_VIN jack). Power is supplied to the [[ADI>CN0393|EVAL-CN0393-FMCZ]] hardware via the FMC connector, but is not activated until the [[ftp://ftp.analog.com/pub/cftl/CN0393|CN-0393 Evaluation Software]] runs and configures the hardware. | - After connecting the [[ADI>CN0393|EVAL-CN0393-FMCZ]] and [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/eval-sdp-h1.html|EVAL-SDP-CH1Z]] boards, connect the +12 V switched mode power supply to the [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/eval-sdp-h1.html|EVAL-SDP-CH1Z]] board (via the +12V_VIN jack). Power is supplied to the [[ADI>CN0393|EVAL-CN0393-FMCZ]] hardware via the FMC connector, but is not activated until the [[ftp://ftp.analog.com/pub/cftl/CN0393|CN-0393 Evaluation Software]] runs and configures the hardware. |
- Connect the hardware to the PC via the USB cable. If the **ADI SDP Drivers** are already installed, the connection to the [[http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/eval-sdp-h1.html|EVAL-SDP-CH1Z]] (SDP-H1) board can be verified by checking Device Manager (appears under ADI Development Tools). | - Connect the hardware to the PC via the USB cable. If the **ADI SDP Drivers** are already installed, the connection to the [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/eval-sdp-h1.html|EVAL-SDP-CH1Z]] (SDP-H1) board can be verified by checking Device Manager (appears under ADI Development Tools). |
| |
===== Using the Evaluation Software ===== | ===== Using the Evaluation Software ===== |
| |
The [[ftp://ftp.analog.com/pub/cftl/CN0393|CN-0393 Evaluation Software]] interfaces with the [[http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/eval-sdp-h1.html|EVAL-SDP-CH1Z]] and [[ADI>CN0393|EVAL-CN0393-FMCZ]] hardware. It can be used to connect to the hardware, configure the channel gains and execute conversions to evaluate the CN-0393 reference design. The front panel and various tab controls provide access to key system parameters and controls for collecting, processing, and viewing results. Waveform, histogram, and FFT plots are included for quick time- and frequency-domain analysis. | The [[ftp://ftp.analog.com/pub/cftl/CN0393|CN-0393 Evaluation Software]] interfaces with the [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/eval-sdp-h1.html|EVAL-SDP-CH1Z]] and [[ADI>CN0393|EVAL-CN0393-FMCZ]] hardware. It can be used to connect to the hardware, configure the channel gains and execute conversions to evaluate the CN-0393 reference design. The front panel and various tab controls provide access to key system parameters and controls for collecting, processing, and viewing results. Waveform, histogram, and FFT plots are included for quick time- and frequency-domain analysis. |
| |
The software also allows for standalone operation without the hardware connected. In this mode, the software can load previously saved results for analysis and viewing. | The software also allows for standalone operation without the hardware connected. In this mode, the software can load previously saved results for analysis and viewing. |
* **FFT Tab**: Shows frequency-domain results from the CN-0393 hardware. | * **FFT Tab**: Shows frequency-domain results from the CN-0393 hardware. |
* **Summary Tab**: Shows summary of results from the CN-0393 hardware. | * **Summary Tab**: Shows summary of results from the CN-0393 hardware. |
* **Reference Voltage (V)**: Set to the reference voltage being used on the hardware. This value is used to calculate the various analysis items in the **Waveform**, **Histogram**, **FFT**, and **Summary** tabs. Does not change the reference being used on the board. The CN-0393 hardware is set to 5 V by default. | * **Reference Voltage (V)**: Set to the reference voltage being used on the hardware. This value is used to calculate the various analysis items in the **Waveform**, **Histogram**, **FFT**, and **Summary** tabs. When this value is changed, it will update the analysis items and input range indicators for each channel; however, it does **not** change the reference being used on the board. As such, users should take care to make sure this control matches the actual reference voltage used on-board. The CN-0393 hardware is set to 5 V by default (using the [[ADI>ADR4550]]. |
* **Sampling Rate (kSPS)**: Set to the desired sample rate to be used on the CN-0393 hardware, in kSPS. The maximum sample rate is 500 kSPS. | * **Sampling Rate (kSPS)**: Set to the desired sample rate to be used on the CN-0393 hardware, in kSPS. The maximum sample rate is 500 kSPS. |
* **SCK Freq (MHz)**: Set to the desired SCK frequency to be used on the CN-0393 hardware, in MHz. The maximum SCK frequency is 40 MHz. | * **SCK Freq (MHz)**: Set to the desired SCK frequency to be used on the CN-0393 hardware, in MHz. The maximum SCK frequency is 40 MHz. |
* **CA Gain**: Sets the gain of Channel A on the CN-0393 hardware. | * **CA Gain**: Sets the gain of Channel A on the CN-0393 hardware. |
* **CB Gain**: Sets the gain of Channel B on the CN-0393 hardware. | * **CB Gain**: Sets the gain of Channel B on the CN-0393 hardware. |
* **CA Input Range**: Displays the current input range of Channel A on the CN-0393 hardware. This value is determined by the Channel A gain setting (**CA Gain**). | * **CA Input Range**: Displays the current input range of Channel A on the CN-0393 hardware. This value is determined by the Channel A gain setting (**CA Gain**) and **Reference Voltage (V)**. |
* **CB Input Range**: Displays the current input range of Channel B on the CN-0393 hardware. This value is determined by the Channel B gain setting (**CB Gain**). | * **CB Input Range**: Displays the current input range of Channel B on the CN-0393 hardware. This value is determined by the Channel B gain setting (**CB Gain**) and **Reference Voltage (V)**. |
* **Flash LED**: Flashes the STATUS LED on the SDP-H1 board. | * **Flash LED**: Flashes the STATUS LED on the SDP-H1 board. |
| |
* **Reinitialize Default Values**: Reinitializes the software to its start-up state. | * **Reinitialize Default Values**: Reinitializes the software to its start-up state. |
== Help == | == Help == |
* **Analog Devices Website (Ctrl + W)**: Opens the [[http://www.analog.com/en/index.html|Analog Devices website]] in the default browser. | * **Analog Devices Website (Ctrl + W)**: Opens the [[adi>en/index.html|Analog Devices website]] in the default browser. |
* **CN-0393 Product Page**: Opens the [[ADI>CN-0393]] product page in the default browser. | * **CN-0393 Product Page**: Opens the [[ADI>CN0393]] product page in the default browser. |
* **User Guide (Ctrl + D)**: Opens the [[ftp://ftp.analog.com/pub/cftl/CN0393|CN-0393 Evaluation Software]] wiki-based [[https://wiki.analog.com/resources/eval/user-guides/circuits-from-the-lab/cn0393|User Guide]] in the default browser. | * **User Guide (Ctrl + D)**: Opens the [[ftp://ftp.analog.com/pub/cftl/CN0393|CN-0393 Evaluation Software]] wiki-based [[/resources/eval/user-guides/circuits-from-the-lab/cn0393|User Guide]] in the default browser. |
* **Context Help (Ctrl + H)**: Opens the context help box. This box displays descriptions of the objects in the software as the mouse hovers over them. | * **Context Help (Ctrl + H)**: Opens the context help box. This box displays descriptions of the objects in the software as the mouse hovers over them. |
* **About**: Displays version information about the software. | * **About**: Displays version information about the software. |
=== Establishing Hardware USB Connection Link === | === Establishing Hardware USB Connection Link === |
Once the [[ADI>CN0393|EVAL-CN0393-FMCZ]] and [[http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/eval-sdp-h1.html|EVAL-SDP-CH1Z]] evaluation boards are connected to the PC and powered up, the [[ftp://ftp.analog.com/pub/cftl/CN0393|CN-0393 Evaluation Software]] can be run and establish a USB connection to the hardware. See **Hardware Setup** for instructions on setting up the hardware. | Once the [[ADI>CN0393|EVAL-CN0393-FMCZ]] and [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/eval-sdp-h1.html|EVAL-SDP-CH1Z]] evaluation boards are connected to the PC and powered up, the [[ftp://ftp.analog.com/pub/cftl/CN0393|CN-0393 Evaluation Software]] can be run and establish a USB connection to the hardware. See **Hardware Setup** for instructions on setting up the hardware. |
| |
To establish a USB connection link between the software and hardware: | To establish a USB connection link between the software and hardware: |
- If the USB connection to the hardware is lost at any point during operation, a pop-up will appear to indicate this. Selecting **Rescan** will attempt to reestablish the USB connection. Selecting **Cancel** will instruct the software to run in standalone mode (see **Standalone Mode**). | - If the USB connection to the hardware is lost at any point during operation, a pop-up will appear to indicate this. Selecting **Rescan** will attempt to reestablish the USB connection. Selecting **Cancel** will instruct the software to run in standalone mode (see **Standalone Mode**). |
=== Configuring Channel Gains === | === Configuring Channel Gains === |
The [[ADI>CN-0393]] hardware allows for software-controlled channel gain setting for the two data acquisition channels (channels A and B). It does this by setting the gain address pins on each channel’s [[ADI>AD8251]]s. These gains are configured via the **CA Gain** and **CB Gain** controls in the **Configuration Tab**. **CA Gain** and **CB Gain** set the gains for channels A and B, respectively. When a new gain is selected for either control, the hardware updates the respective channel’s [[ADI>AD8251]] gain setting. When the update is complete, the **Status** bar will display the current gain settings and input ranges for both channels. The **CA Input Range** and **CB Input Range** indicators also show the corresponding input ranges for the current channel gain settings. | The [[ADI>CN0393]] hardware allows for software-controlled channel gain setting for the two data acquisition channels (channels A and B). It does this by setting the gain address pins on each channel’s [[ADI>AD8251]]s. These gains are configured via the **CA Gain** and **CB Gain** controls in the **Configuration Tab**. **CA Gain** and **CB Gain** set the gains for channels A and B, respectively. When a new gain is selected for either control, the hardware updates the respective channel’s [[ADI>AD8251]] gain setting. When the update is complete, the **Status** bar will display the current gain settings and input ranges for both channels. The **CA Input Range** and **CB Input Range** indicators also show the corresponding input ranges for the current channel gain settings. |
=== Capturing Samples === | === Capturing Samples === |
Capturing results/samples can be performed by pressing either the **Single Capture** or **Continuous Capture** controls on the software’s front panel. The **Single Capture** button performs a single set of conversions, and **Continuous Capture** performs repeated sets of conversions. The number of samples in the set of conversions in determined by the **Num Samples** control. For example, if **Num Samples** is set to 8192, then 8192 conversions will be performed, resulting in 8192 results for each channel. Results can be viewed on the **Waveform**, **Histogram**, **FFT**, and **Summary** tabs after the conversions are executed (see **Viewing Results**). | Capturing results/samples can be performed by pressing either the **Single Capture** or **Continuous Capture** controls on the software’s front panel. The **Single Capture** button performs a single set of conversions, and **Continuous Capture** performs repeated sets of conversions. The number of samples in the set of conversions in determined by the **Num Samples** control. For example, if **Num Samples** is set to 8192, then 8192 conversions will be performed, resulting in 8192 results for each channel. Results can be viewed on the **Waveform**, **Histogram**, **FFT**, and **Summary** tabs after the conversions are executed (see **Viewing Results**). |
The [[ftp://ftp.analog.com/pub/cftl/CN0393|CN-0393 Evaluation Software]] can operate in “standalone” mode when the evaluation hardware is not connected. In this mode, the software cannot initiate new conversions, but it can load previous sets of conversion results (see **Loading and Saving Results**). | The [[ftp://ftp.analog.com/pub/cftl/CN0393|CN-0393 Evaluation Software]] can operate in “standalone” mode when the evaluation hardware is not connected. In this mode, the software cannot initiate new conversions, but it can load previous sets of conversion results (see **Loading and Saving Results**). |
| |
Standalone mode is initiated when the evaluation software does not establish a connection with the evaluation hardware, and the user selects **Cancel** in the pop-up that appears. This can occur at start-up or if the software loses an established connection with the hardware. A pop-up will appear to indicate when software enters standalone mode. {{ :resources:eval:user-guides:circuits-from-the-lab:cn0393_standalone_notification.png?600 |}} | Standalone mode is initiated when the evaluation software does not establish a connection with the evaluation hardware, and the user selects **Cancel** in the pop-up that appears. This can occur at start-up or if the software loses an established connection with the hardware. A pop-up will appear to indicate when software enters standalone mode. {{ :resources:eval:user-guides:circuits-from-the-lab:cn0393_standalone_notification.png?800 |}} |
| |
The software will exit standalone mode if it can establish or reestablish a connection to the hardware (see **Establishing Hardware USB Connection Link**). | The software will exit standalone mode if it can establish or reestablish a connection to the hardware (see **Establishing Hardware USB Connection Link**). |
| |