Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision |
resources:eval:user-guides:circuits-from-the-lab:cn0372 [10 Jul 2018 20:32] – [More Information and Useful Links] Motoko Hunt | resources:eval:user-guides:circuits-from-the-lab:cn0372 [03 Jan 2021 22:03] – fix links Robin Getz |
---|
The [[ADI>AD7091R-5]] accepts the analog signals, buffered or unbuffered, and performs data conversion. The [[ADI>ADA4805-1]] is an optional buffer which can be used for all input channels because of an access to the multiplexer output of the [[ADI>AD7091R-5]]. The [[ADI>ADP5090]] harvests charge from a photovoltaic cell to generate the system DC supply rails. Another option provided to power the board is with the [[ADI>ADP1607]]. A CR2032 battery connector is available to provide either the input to the [[ADI>ADP1607]] or accelerate the cold start of the [[ADI>ADP5090]]. | The [[ADI>AD7091R-5]] accepts the analog signals, buffered or unbuffered, and performs data conversion. The [[ADI>ADA4805-1]] is an optional buffer which can be used for all input channels because of an access to the multiplexer output of the [[ADI>AD7091R-5]]. The [[ADI>ADP5090]] harvests charge from a photovoltaic cell to generate the system DC supply rails. Another option provided to power the board is with the [[ADI>ADP1607]]. A CR2032 battery connector is available to provide either the input to the [[ADI>ADP1607]] or accelerate the cold start of the [[ADI>ADP5090]]. |
| |
This user guide will discuss how to operate the [[http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL_SDP-PMOD.html#eb-overview| SDP-PMD-IB1Z]], [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] and the evaluation software to configure and collect data from the EVAL-CN0372-PMDZ Evaluation Board (**CN0372 Board**). The evaluation board also has PMOD and IMOD compatible headers which allows for connection to other processors or microcontrollers. | This user guide will discuss how to operate the [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL_SDP-PMOD.html#eb-overview| SDP-PMD-IB1Z]], [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] and the evaluation software to configure and collect data from the EVAL-CN0372-PMDZ Evaluation Board (**CN0372 Board**). The evaluation board also has PMOD and IMOD compatible headers which allows for connection to other processors or microcontrollers. |
| |
A complete design support package for the [[adi>EVAL-CN0372-PMDZ]] evaluation board containing schematics, layouts (native and Gerber), and bill-of-materials can be found at: [[http://www.analog.com/CN0372-DesignSupport|CN0372-DesignSupport]]. | A complete design support package for the [[adi>EVAL-CN0372-PMDZ]] evaluation board containing schematics, layouts (native and Gerber), and bill-of-materials can be found at: [[adi>CN0372-DesignSupport|CN0372-DesignSupport]]. |
| |
{{:resources:eval:user-guides:circuits-from-the-lab:cn0372:1.png?direct&600|}} | {{:resources:eval:user-guides:circuits-from-the-lab:cn0372:1.png?direct&600|}} |