This version is outdated by a newer approved version.This version (17 Mar 2015 15:59) is a draft.
Approvals: 0/1
This is an old revision of the document!
Magneto-Resistive Angle and Linear Position Measurements (CN0368)
Overview
This circuit provides a contactless, AMR (Anisotropic Magneto Resistive) based angle measurement solution ideal for angle and linear position measurements. The system is capable of providing better than 0.2 degree accuracy. This translates into a linear position accuracy of 2 mil (0.002 inches).
The circuit is ideal for applications where high speed, accurate, non-contact angle and length measurements are critical such as brushless DC motor control.
General Setup
Minimum PC/System Requirements
How to Install the Evaluation Software
Extract the files within the file
CN0368 SDP Eval Software.zip and open the file
setup.exe. It is recommended that you install the CN0368 SDP Evaluation Software to the default directory path
C:\Program Files\Analog Devices\CN0368\ and all National Instruments products to
C:\Program Files\National Instruments\
Press
“Next”.
Press
“Next”.
Press “Next”.
Upon completion of the installation of the
CN0368 SDP Eval Software, the installer for the
ADI SDP Drivers will execute. Follow the on-screen prompts to install the drivers. It is recommended that you close all other applications before clicking “Next”. This will make it possible to update relevant system files without having to reboot your computer.
-
Press “Next”.
-
It is recommended that you install the drivers to the default directory path C:\Program Files\Analog Devices\SDP\Drivers\
Press “Install” to install the Drivers and complete the installation of all software necessary to evaluate the EVAL-CN0368-SDPZ
Opening and Enabling the Evaluation Software
Launch the executable found at C:\Program Files\Analog Devices\CN0368 and press the “Connect“ button.
-
Step by Step Instruction for Calibrating the System
The following is a step by step guide for manual or automatic calibration of the calibrating the EVAL-CN0368-SDPZ.
A manual calibration requires the user to input the maximum and minimum ADC code for each channel of the ADC.
An automatic calibration allows the software to identify the maximum and minimum ADC code for each channel of the ADC. This method is easier to use than the manual method, however, it may introduce errors if the magnet is spinning with an un-smooth or non-periodic nature.
-
Step 1: Begin by selecting manual or automatic calibration.
Step 2: Press the 'Click to Sample' button to begin data conversion.
Step 3: Rotate the magnet and observe the changing ADC codes.
Step 4: If manual calibration was selected, you must input the maximum and minimum codes (seen in step 3) in the boxes provided. If automatic calibration was selected, you must simply spin the magnet through several complete revolutions to allow the software to identify the necessary codes.
The calibration coefficients can be modified to produce a better end result. For example, if one of the maximum ADC codes is mis-represented on the high side, the output angle will never reach +90 degrees or -90 degrees depending on the channel.
Once the calibration is complete, proceed to the second tab 'Final Angle(Needle)' to observe the angle information.