This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0368 [30 Mar 2015 20:42] – [Step by Step Instruction for Calibrating the System] Neil Wilson | resources:eval:user-guides:circuits-from-the-lab:cn0368 [30 Mar 2015 21:22] – [Multiple Temperature Calibration] Neil Wilson | ||
---|---|---|---|
Line 42: | Line 42: | ||
The Single Temperature Calibration method allows the user to calculate VSIN_Offset and VCOS_Offset before calculating the magnetic field angle. | The Single Temperature Calibration method allows the user to calculate VSIN_Offset and VCOS_Offset before calculating the magnetic field angle. | ||
- Select ' | - Select ' | ||
- | - | + | - {{: |
- A prompt will appear instructing the user to rotate the magnetic stimulus through 360 degrees. | - A prompt will appear instructing the user to rotate the magnetic stimulus through 360 degrees. | ||
- In this time the software is actively calculating VSIN_Offset and VCOS_Offset. | - In this time the software is actively calculating VSIN_Offset and VCOS_Offset. | ||
- Press ' | - Press ' | ||
+ | - The software will display the magnetic field angle, VSIN_Offset, | ||
- Press ' | - Press ' | ||
- | + | - {{: | |
+ | - Press ' | ||
==== Multiple Temperature Calibration ==== | ==== Multiple Temperature Calibration ==== | ||
+ | The Multiple Temperature Calibration procedure is a method of compensating for temperature effects experienced by the amplifier and ADC. The temperature coefficients and offsets are calculated to provide a more accurate magnetic field angle and system response. | ||
+ | - Select // | ||
+ | - Place the hardware in a temperature controlled environment at the desired T1. | ||
+ | - {{: | ||
+ | - Press // | ||
+ | - {{: | ||
+ | - Rotate the stimulus through 360 degrees while VSIN_Offset_T1 and VCOS_Offset_T1 are calculated. | ||
+ | - Press // | ||
+ | - {{: | ||
+ | - Place the hardware in a temperature controlled environment at the desired T2. | ||
+ | - Press // | ||
+ | - {{: | ||
+ | - Rotate the stimulus through 360 degrees while VSIN_Offset_T2 and VCOS_Offset_T2 are calculated. | ||
+ | - Press // | ||
+ | - Press //**Sample Data**// to observe the magnetic field angle results corrected for temperature and offset effects. | ||
==== Dynamic Calibration ==== | ==== Dynamic Calibration ==== | ||
The Dynamic Calibration method actively calculates VSIN_Offset and VCOS_Offset as the magnetic stimulus rotates through 360 degrees. | The Dynamic Calibration method actively calculates VSIN_Offset and VCOS_Offset as the magnetic stimulus rotates through 360 degrees. |