This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0359 [13 Jul 2017 05:17] – [RS-485 command usage] Robert Lee | resources:eval:user-guides:circuits-from-the-lab:cn0359 [29 Jul 2021 09:13] – Hardware Registration Harvey John De Chavez | ||
---|---|---|---|
Line 125: | Line 125: | ||
The CN0359 system runs using a 6V DC wall connector (EVAL-CFTL-6V-PWRZ) and will run automatically when the power on. The system has two interfaces to show the conductivity and RTD results: LCD screen and RS-485 interface, and those two interfaces can working simultaneously as well. | The CN0359 system runs using a 6V DC wall connector (EVAL-CFTL-6V-PWRZ) and will run automatically when the power on. The system has two interfaces to show the conductivity and RTD results: LCD screen and RS-485 interface, and those two interfaces can working simultaneously as well. | ||
- | <note tip>The CN0359 usage is depend on the software version, maybe there have difference between following instructions and shipped CN0359, please check [[http:// | + | <note tip>The CN0359 usage is depend on the software version, maybe there have difference between following instructions and shipped CN0359, please check [[adi>cn0359-DesignSupport]] for latest software update download</ |
The CN0359 has the following opinions which can be set by the user: | The CN0359 has the following opinions which can be set by the user: | ||
Line 387: | Line 387: | ||
- Download latest [[https:// | - Download latest [[https:// | ||
- | - Download latest [[http:// | + | - Download latest [[adi>cn0359-designsupport|CN0359 Design & Integration Files]] to your computer hard disk |
- Install J-Link Software and Documentation Pack to your computer following the instructions in package | - Install J-Link Software and Documentation Pack to your computer following the instructions in package | ||
- Extract //CN0359 Design & Integration Files// to your computer hard disk | - Extract //CN0359 Design & Integration Files// to your computer hard disk | ||
Line 448: | Line 448: | ||
===== Software development environment ===== | ===== Software development environment ===== | ||
- | The CN0359 software source code could be download at: [[http:// | + | The CN0359 software source code could be download at: [[adi>CN0359-DesignSupport]], |
The tools for CN0359 development could be downloaded at following list: | The tools for CN0359 development could be downloaded at following list: | ||
Line 614: | Line 614: | ||
* Software (setup and hold time setting added) | * Software (setup and hold time setting added) | ||
* Software (RS-485 communication routines added) | * Software (RS-485 communication routines added) | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | </ |