This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0359 [03 Dec 2018 18:35] – [How to download binary firmware to the CN0359] Nasser Shabbir | resources:eval:user-guides:circuits-from-the-lab:cn0359 [03 Jan 2021 21:55] – fix links Robin Getz | ||
---|---|---|---|
Line 125: | Line 125: | ||
The CN0359 system runs using a 6V DC wall connector (EVAL-CFTL-6V-PWRZ) and will run automatically when the power on. The system has two interfaces to show the conductivity and RTD results: LCD screen and RS-485 interface, and those two interfaces can working simultaneously as well. | The CN0359 system runs using a 6V DC wall connector (EVAL-CFTL-6V-PWRZ) and will run automatically when the power on. The system has two interfaces to show the conductivity and RTD results: LCD screen and RS-485 interface, and those two interfaces can working simultaneously as well. | ||
- | <note tip>The CN0359 usage is depend on the software version, maybe there have difference between following instructions and shipped CN0359, please check [[http:// | + | <note tip>The CN0359 usage is depend on the software version, maybe there have difference between following instructions and shipped CN0359, please check [[adi>cn0359-DesignSupport]] for latest software update download</ |
The CN0359 has the following opinions which can be set by the user: | The CN0359 has the following opinions which can be set by the user: | ||
Line 387: | Line 387: | ||
- Download latest [[https:// | - Download latest [[https:// | ||
- | - Download latest [[http:// | + | - Download latest [[adi>cn0359-designsupport|CN0359 Design & Integration Files]] to your computer hard disk |
- Install J-Link Software and Documentation Pack to your computer following the instructions in package | - Install J-Link Software and Documentation Pack to your computer following the instructions in package | ||
- Extract //CN0359 Design & Integration Files// to your computer hard disk | - Extract //CN0359 Design & Integration Files// to your computer hard disk | ||
Line 448: | Line 448: | ||
===== Software development environment ===== | ===== Software development environment ===== | ||
- | The CN0359 software source code could be download at: [[http:// | + | The CN0359 software source code could be download at: [[adi>CN0359-DesignSupport]], |
The tools for CN0359 development could be downloaded at following list: | The tools for CN0359 development could be downloaded at following list: |