This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0357 [03 Jan 2021 21:55] – fix links Robin Getz | resources:eval:user-guides:circuits-from-the-lab:cn0357 [15 Aug 2022 03:52] – Updated download link for the CN0357 Evaluation Software. Allan Uy | ||
---|---|---|---|
Line 17: | Line 17: | ||
* [[adi> | * [[adi> | ||
* [[adi> | * [[adi> | ||
- | * [[ftp://ftp.analog.com/ | + | * [[http://swdownloads.analog.com/ |
- | * (supplied with provided CD in kit) | + | |
* PC with the following //Minimum Requirements// | * PC with the following //Minimum Requirements// | ||
* Windows XP Service Pack 2 (32-bit) | * Windows XP Service Pack 2 (32-bit) | ||
Line 133: | Line 132: | ||
===== Downloads ===== | ===== Downloads ===== | ||
{{: | {{: | ||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | </ |