Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
Next revisionBoth sides next revision
resources:eval:user-guides:circuits-from-the-lab:cn0357 [12 Aug 2014 20:22] – [Software Control and Indicator Descriptions] James Fitzgeraldresources:eval:user-guides:circuits-from-the-lab:cn0357 [16 Apr 2018 09:49] Jesse Daniel Santos
Line 10: Line 10:
 This user guide will discuss how to use the evaluation software to collect data from the [[http://www.analog.com/EVAL-CN0357-PMDZ|EVAL-CN0357-PMDZ]] Evaluation Board **(CN-0357 Board)** This user guide will discuss how to use the evaluation software to collect data from the [[http://www.analog.com/EVAL-CN0357-PMDZ|EVAL-CN0357-PMDZ]] Evaluation Board **(CN-0357 Board)**
  
-{{:resources:eval:user-guides:circuits-from-the-lab:cn0357:cn0357-simplified_schematic.png?nolink&|}}+{{:resources:eval:user-guides:circuits-from-the-lab:cn0357:cn0357-simplified_schematic.png?800|}} 
 ===== Required Equipment ===== ===== Required Equipment =====
   * [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**)   * [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**)
Line 29: Line 30:
   * The [[http://www.analog.com/EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V DC Power Supply)** powers the [[http://www.analog.com/SDP-PMD-IB1Z|SDP-PMD-IB1Z]] **(SDP to Pmod Interposer Board)** via the DC barrel jack   * The [[http://www.analog.com/EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V DC Power Supply)** powers the [[http://www.analog.com/SDP-PMD-IB1Z|SDP-PMD-IB1Z]] **(SDP to Pmod Interposer Board)** via the DC barrel jack
   * The [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable.   * The [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable.
-\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0357:cn0357-test_setup.png?nolink&|}} +{{ :resources:eval:user-guides:circuits-from-the-lab:cn0357:cn0357-test_setup.png?nolink |}}
 ---- ----
 ===== Installing the Software ===== ===== Installing the Software =====
Line 71: Line 71:
     * __Reduction (source)__ - Select this option if the sensor sources current.      * __Reduction (source)__ - Select this option if the sensor sources current. 
   -**Max Sensor Sensitivity Numerical Control**   -**Max Sensor Sensitivity Numerical Control**
-    * The maximum amount of current in nanoamps (nA) the sensor will sink/source per part per million (ppm).  This control influences the feedback resistance set by the Rheostat ([[http://www.analog.com/AD5270|AD5270]]).+    * The maximum amount of current in nanoamps (nA) the sensor will sink/source per part per million (ppm).   
 +    * This control influences the feedback resistance set by the Rheostat ([[http://www.analog.com/AD5270|AD5270]]).
   -**Typical Sensor Sensitivity Drop-down Menu**   -**Typical Sensor Sensitivity Drop-down Menu**
-    * The typical amount of current in nanoamps (nA) the sensor will sink/source per part per million (ppm).  This control influences the size of the LSB in terms of ppm/mV and mV/ppm.+    * The typical amount of current in nanoamps (nA) the sensor will sink/source per part per million (ppm). 
 +    * This control influences the size of the LSB in terms of ppm/mV and mV/ppm.
   -**Sensor Range Numerical Control**   -**Sensor Range Numerical Control**
     * The maximum concentration the sensor can measure in parts per million.     * The maximum concentration the sensor can measure in parts per million.
   -**Feedback Resistance Numerical Indicator**   -**Feedback Resistance Numerical Indicator**
-    * The feedback resistance of the transimpedance amplifier on the **CN0357 Board** ([[http://www.analog.com/ADA4528-2|ADA4528-2]]).  This can be set by the Rheostat ([[http://www.analog.com/AD5270|AD5270]]) or by populating a fixed resistor in the available footprint.+    * The feedback resistance of the transimpedance amplifier on the **CN0357 Board** ([[http://www.analog.com/ADA4528-2|ADA4528-2]]). 
 +    * This can be set by the Rheostat ([[http://www.analog.com/AD5270|AD5270]]) or by populating a fixed resistor in the available footprint.
   -**ppm/mV Numerical Indicator**   -**ppm/mV Numerical Indicator**
     * Parts per million concentration per millavolt     * Parts per million concentration per millavolt
Line 91: Line 94:
     * This indicator displays the current state of the software in the form of an LED.  There are three status LED colors.\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0357:cn0357-software-inactive.png?nolink&|}}Inactive\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0357:cn0357-software-busy.png?nolink&|}}Busy\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0357:cn0357-software-error.png?nolink&|}}Error\\      * This indicator displays the current state of the software in the form of an LED.  There are three status LED colors.\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0357:cn0357-software-inactive.png?nolink&|}}Inactive\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0357:cn0357-software-busy.png?nolink&|}}Busy\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0357:cn0357-software-error.png?nolink&|}}Error\\ 
   -**Buffer Mode Radio Buttons**   -**Buffer Mode Radio Buttons**
-    * __Buffered Mode__ - FIXME +    * __Buffered Mode__ - This allows the user to place source impedance on the front end without contributing to gain errors to the system. 
-    * __Unbuffered Mode__ - FIXME+    * __Unbuffered Mode__ - This disables the buffers, lowering the power consumption of the device.\\ \\ <WRAP center round info 60%> \\ Enabling the buffers also reduces the **Analog Input Range** of the ADC</WRAP>
   -**Mode Register Numerical Indicator**   -**Mode Register Numerical Indicator**
-    * FIXME+    * This register is used to configure the ADC for range, enable or disable the buffer, or place the device into power-down mode. 
 +    * The **Register Bit Designations** can be found on Page 11 of the [[http://www.analog.com/AD7790|AD7790]] Datasheet in Table 9.
   -**Filter Register Numerical Indicator**   -**Filter Register Numerical Indicator**
-    * FIXME+    * This register is used to set the output word rate.  
 +    * Table 12 in the [[http://www.analog.com/AD7790|AD7790]] Datasheet outlines the **Register Bit Designations** for the filter register.\\ \\ <WRAP center round info 60%> \\ The CN0357 Evaluation Software uses the **Single Conversion Mode**.</WRAP>
   -**Reset ADC Button**   -**Reset ADC Button**
-    * FIXME+    * The serial interface can be reset by writing a series of 1s on the DIN input. 
 +    * Reset returns the interface to the state in which it is expecting a write to the communications register. 
 +    * This operation resets the contents of all registers to their power-on values.
   -**Feedback Selector Radio Buttons**   -**Feedback Selector Radio Buttons**
-    * __Rheostat__ - FIXME +    * __Rheostat__ - Selecting this option uses the Rheostat for the feedback resistance of the transimpedance amplifier and disables the **Fixed Resistor Numerical Control**. 
-    * __Fixed Resistor__ - FIXME+    * __Fixed Resistor__ - Selecting this option uses a fixed-resistor for the feedback resistance of the transimpedance amplifier and disables the **RDAC Value Numerical Indicator**, **Rheostat Resistance Numerical Indicator** and **Program Rheostat Button**.
   -**Fixed Resistor Numerical Control**   -**Fixed Resistor Numerical Control**
-    * FIXME+    * Input the value of the resistor populated at **R7** if not using the Rheostat
   -**RDAC Value Numerical Indicator**   -**RDAC Value Numerical Indicator**
-    * FIXME+    * The value transmitted to the RDAC register of the Rheostat in hexadecimal format.
   -**Rheostat Resistance Numerical Indicator**   -**Rheostat Resistance Numerical Indicator**
-    * FIXME+    * The equivalent resistance of the Rheostat. 
   -**Program Rheostat Button**   -**Program Rheostat Button**
-    * FIXME+    * Load the current RDAC value to the 50-TP Memory Block of the Digital Rheostat.\\ \\ <WRAP center round important 60%>\\ Programming the current RDAC value to 50-TP can only occur 50 times.</WRAP> 
  
 ---- ----
-==== Capturing a Data ==== +==== Running the System ==== 
-FIXME +  - Open the **CN0357.exe** application from the default installation location. 
-  - **Establish a USB Connection Link**.+  - The software will connect to the board automatically.
   - Click the **Run Button**   - Click the **Run Button**
   - Click the **Stop Button** when acquisition is complete.   - Click the **Stop Button** when acquisition is complete.
 ==== Saving Data to a Spreadsheet File ==== ==== Saving Data to a Spreadsheet File ====
-  - **Capture Data**. 
   - Click the **Save Data Button**.   - Click the **Save Data Button**.
   - Browse to the directory location where the spreadsheet file is to be saved.   - Browse to the directory location where the spreadsheet file is to be saved.
   - Name the file.   - Name the file.
   - Click the **OK Button**.   - Click the **OK Button**.
-<WRAP left round info 60%>\\ The software saves the spreadsheet file as ASCII text with columns separated by tabs.</WRAP>+<WRAP center round info 60%>\\ The software saves the spreadsheet file as ASCII text with columns separated by tabs</WRAP>
 ===== Downloads ===== ===== Downloads =====
 {{:resources:eval:user-guides:circuits-from-the-lab:cn0357:cn0357-labview_source.zip|CN0357 LabVIEW Source}} {{:resources:eval:user-guides:circuits-from-the-lab:cn0357:cn0357-labview_source.zip|CN0357 LabVIEW Source}}
resources/eval/user-guides/circuits-from-the-lab/cn0357.txt · Last modified: 15 Aug 2022 03:59 by Allan Uy