This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0348 [03 Jan 2021 21:55] – fix links Robin Getz | resources:eval:user-guides:circuits-from-the-lab:cn0348 [10 Feb 2021 14:45] – [Required Equipment] - fix link Robin Getz | ||
---|---|---|---|
Line 19: | Line 19: | ||
* SMB Connector | * SMB Connector | ||
* For INL/DNL data collection: | * For INL/DNL data collection: | ||
- | * GPIB Controller for Hi-Speed USB Type A Connector Cable (NI-488.2 3.1.1 GPIB controller driver is available at[[http://joule.ni.com/ | + | * GPIB Controller for Hi-Speed USB Type A Connector Cable (NI-488.2 3.1.1 GPIB controller driver is available at [[https://www.ni.com/en-us/support/model.gpib-usb-hs.html]] |
* Agilent 3458A\\ \\ <WRAP round info 60%>\\ **__NOTE__** - Any multimeter can be used with this board. However, for INL/DNL measurement, | * Agilent 3458A\\ \\ <WRAP round info 60%>\\ **__NOTE__** - Any multimeter can be used with this board. However, for INL/DNL measurement, | ||