This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0341 [05 Jan 2021 16:24] – Removed old references Ioana Chelaru | resources:eval:user-guides:circuits-from-the-lab:cn0341 [04 Apr 2024 10:16] (current) – [CN0341 -- Magneto Resistive Linear Position Measurement User Guide (DEPRECATED)] Joyce Velasco | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Magneto Resistive Linear Position Measurement (CN0341) ====== | + | ====== |
+ | |||
+ | |||
+ | <WRAP round important 70%> | ||
+ | This reference design has been **RETIRED** or **DEPRECATED**, | ||
+ | \\ | ||
+ | </ | ||
===== Overview ===== | ===== Overview ===== | ||
Line 6: | Line 12: | ||
*One EVAL-CN0341-SDPZ Evaluation Board | *One EVAL-CN0341-SDPZ Evaluation Board | ||
*[[adi> | *[[adi> | ||
- | *[[ftp:// | + | *CN0341 Evaluation Software |
*One USB Type-A plug to USB Mini-B plug cable. | *One USB Type-A plug to USB Mini-B plug cable. | ||
*One Neodymium magnet, approximately two inches in length. magnetized along the length of the magnet. | *One Neodymium magnet, approximately two inches in length. magnetized along the length of the magnet. | ||
Line 58: | Line 64: | ||
- The image below displays one last common error source, sensor-to-magnet distance. The ideal distance between the sensor and magnet is half of the magnet length. Increasing or decreasing this distance introduces errors into the measurement. | - The image below displays one last common error source, sensor-to-magnet distance. The ideal distance between the sensor and magnet is half of the magnet length. Increasing or decreasing this distance introduces errors into the measurement. | ||
- {{ : | - {{ : | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | </ |