This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0336 [01 Oct 2013 21:58] – complete Christo Hrisulev | resources:eval:user-guides:circuits-from-the-lab:cn0336 [07 Jun 2018 04:54] – Jesse Daniel Santos | ||
---|---|---|---|
Line 10: | Line 10: | ||
{{ : | {{ : | ||
+ | |||
+ | Figure 1. 4 mA to 20 mA Single Supply Analog to Digital Conversion with Isolation (All Connections and Decoupling Not Shown) | ||