This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0336 [07 Jun 2018 04:54] – Jesse Daniel Santos | resources:eval:user-guides:circuits-from-the-lab:cn0336 [03 Jan 2021 21:56] – fix links Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== CN0336 Software User Guide ====== | ====== CN0336 Software User Guide ====== | ||
===== Overview===== | ===== Overview===== | ||
- | [[http:// | + | [[ADI>CN0336]] provides robust and complete solution for 4 mA-to-20 mA current to digital conversion with isolation, for wide variety measurements where, sensors with standard 4-20 mA output are used. The design solution is optimized for high precision and low cost measurement, |
- | The circuit shown in Figure 1 incorporates [[http:// | + | The circuit shown in Figure 1 incorporates [[ADI>AD8606ARZ]] OpAmp, [[ADI>AD7091RBRMZ]] 12-bit successive approximation (SAR) ADC, and [[ADI>ADuM5401ARWZ]] isolator to create a standard 4 mA-to-20mA current measurement system. |
The circuit has 12 pin PMOD connector on board, which could be used for connection to a customer microprocessor or FPGA. | The circuit has 12 pin PMOD connector on board, which could be used for connection to a customer microprocessor or FPGA. | ||
- | This [[http:// | + | This [[ADI>CN0336]] circuit note discusses the design steps needed to optimize the circuit shown in Figure 1 for a specific bandwidth including noise analysis and component selection considerations. |
- | The performance of the circuit could be demonstrated with the use of Analog Devices SDP controller [[http:// | + | The performance of the circuit could be demonstrated with the use of Analog Devices SDP controller [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] and SDP-to-PMOD Interposer Board [[adi>SDP-PMD-IB1Z|SDP-PMD-IB1Z]], |
- | This user guide will discuss how to use the evaluation software to collect data from the EVAL-CN0336-PMDZ Evaluation Board [[http:// | + | This user guide will discuss how to use the evaluation software to collect data from the EVAL-CN0336-PMDZ Evaluation Board [[adi>CN0336|CN0336]] |
{{ : | {{ : | ||
Line 17: | Line 17: | ||
===== Required Equipment ===== | ===== Required Equipment ===== | ||
- | * [[http:// | + | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**) |
- | * [[http:// | + | * [[adi>EVAL-CN0336-SPMDZ|EVAL-CN0336-PMDZ]] Evaluation Board (**CN-0336 Board**) |
- | * [[http:// | + | * [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V Power Supply)** or equivalent |
- | * [[http:// | + | * [[adi>SDP-PMD-IB1Z]] SDP-to-PMOD interposer board |
* Current Calibrator | * Current Calibrator | ||
* Multimeter(to measure the input current) | * Multimeter(to measure the input current) | ||
Line 32: | Line 32: | ||
* USB type A to USB type mini-B cable | * USB type A to USB type mini-B cable | ||
===== General Setup ===== | ===== General Setup ===== | ||
- | * The [[http:// | + | * The [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V DC Power Supply)** powers the [[adi>EVAL-CN0336-PMDZ|EVAL-CN0336-PMDZ]] **(CN0336 Board)** via the DC barrel jack. |
- | * The [[http:// | + | * The [[adi>SDP-PMD-IB1Z|SDP-PMD-IB1Z]] **(Interposer Board)** connects to the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector A. |
- | * The [[http:// | + | * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. |
- | * The [[http:// | + | * The [[adi>EVAL-CN0336-SDPZ|EVAL-CN0336-SDPZ]] **(CN0336)** connects to the [[adi>EVAL-PMD-IB1Z|EVAL-PMD-IB1Z]] **(Interposer board)** via the 12-Pin header PMOD connector |
- | * The 4-20 mA current source **(Current calibrator)** connects to the [[http:// | + | * The 4-20 mA current source **(Current calibrator)** connects to the [[adi>EVAL-CN0336-SDPZ|EVAL-CN0336-SDPZ]] **(CN0336 Board)** via the terminal block **J2** |
Line 54: | Line 54: | ||
===== Connecting the Hardware ===== | ===== Connecting the Hardware ===== | ||
- | - Connect the [[http:// | + | - Connect the [[adi>EVAL-CFTL-6V-PWRZ|+6V DC Power Supply]] **(Wallwart)** to the barrel jack **J1** of the [[adi>SDP-PMD-IB1Z|Interposer Board ]] **(Interposer Board )** as depicted below.\\ \\ <WRAP left round tip 50%> |
- | - Connect the 120-pin connector on the [[http:// | + | - Connect the 120-pin connector on the [[adi>SDP-PMD-IB1Z|SDP-PMD-IB1Z]] **(Interposer Board)** to the 120-pin connector marked **“CON A”** on the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)**\\ \\ {{: |
- | - Connect the USB cable supplied with [[http:// | + | - Connect the USB cable supplied with [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** to the USB port on the PC and the SDP Board \\ \\ {{: |
- | - Connect the [[http:// | + | - Connect the [[adi>EVAL-CN0336-PMDZ|EVAL-CN0336-PMDZ]] **(CN0336 Board)** to the [[adi>SDP-PMD-IB1Z|SDP-PMD-IB1Z]] **(Interposer Board)** via the 12 pin header PMOD connector. \\ \\ {{: |
- Connect the input current source (Current calibrator) to J2 Terminal Block. The polarity is shown on the picture below \\ {{: | - Connect the input current source (Current calibrator) to J2 Terminal Block. The polarity is shown on the picture below \\ {{: | ||