This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0326 [05 May 2015 19:41] – formatting Brandon Bushey | resources:eval:user-guides:circuits-from-the-lab:cn0326 [03 Jan 2021 21:55] – fix links Robin Getz | ||
---|---|---|---|
Line 10: | Line 10: | ||
===== GENERAL SETUP ===== | ===== GENERAL SETUP ===== | ||
- | * [[http:// | + | * [[adi>EVAL-CN0326-PMDZ|EVAL-CN0326-PMDZ]] Evaluation Board |
- | * [[http:// | + | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Evaluation Board |
- | * [[http:// | + | * [[adi>SDP-PMD-IB1Z|SDP-PMD-IB1Z]] Evaluation Board |
* [[ftp:// | * [[ftp:// | ||
* (supplied with provided CD in kit) | * (supplied with provided CD in kit) | ||
Line 44: | Line 44: | ||
{{: | {{: | ||
- | - Connect | + | - Plug the mini end of the USB cable into connector |
- | - Populate a jumper across JP1 to give +3.3V voltage out in PMOD terminal as seen in the label found in [[http:// | + | * Make sure that the computer installs the device drivers, and that you can see the //ADI Development Tools// in your computer' |
- | - Connect the 12-pin right angle male pin header of [[http:// | + | - Remove the jumper across JP1 found on the [[adi> |
- | - Connect the pH probe in J1 of [[http:// | + | - Connect the 120-pin connector of the [[adi>SDP-PMD-IB1Z|SDP-PMD-IB1Z]] circuit board to the connector marked “CON A” on the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] evaluation (SDP) board. |
- | - Connect the RTD sensor in P1 of [[http:// | + | - Connect the EVAL-CFTL-6V-PWRZ |
- | - Plug the mini end of the USB cable into connector J1 of the [[http:// | + | - Connect the 12-pin right angle male pin header of [[adi>EVAL-CN0326-PMDZ|EVAL-CN0326-PMDZ]] to the 12-pin right angle female pin header of [[adi>SDP-PMD-IB1Z|SDP-PMD-IB1Z]]. |
- | - Plug in the wall wart and connect it to connector J1 of the [[http://www.analog.com/SDP-PMD-IB1Z|SDP-PMD-IB1Z]]. | + | - Connect the pH probe in J1 of [[adi>EVAL-CN0326-PMDZ|EVAL-CN0326-PMDZ]]. |
+ | - Connect the RTD sensor in P1 of [[adi>EVAL-CN0326-PMDZ|EVAL-CN0326-PMDZ]]. | ||
+ | - Place the jumper across JP1 on the [[adi>SDP-PMD-IB1Z|SDP-PMD-IB1Z]] and make sure it's positioned to +3.3V. | ||
+ | - Check again in the device manager | ||
---- | ---- |