Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0303 [05 Jan 2021 16:45] – Removed bad link for CN0303 Ioana Chelaruresources:eval:user-guides:circuits-from-the-lab:cn0303 [29 Jul 2021 07:22] (current) – Hardware Registration Harvey John De Chavez
Line 1: Line 1:
 ====== Vibration Analysis (CN0303) ====== ====== Vibration Analysis (CN0303) ======
 +
 +{{page>/wiki/common#retired&nofooter&noheader}}
 +
 +An [[adi>media/en/reference-design-documentation/reference-designs/CN0303.pdf|archive]] of the circuit note.
  
 ===== Overview ===== ===== Overview =====
Line 39: Line 43:
 ===== Instructions for connecting the ADXL001-70BEZ and EVAL-CN0303_SDPZ ===== ===== Instructions for connecting the ADXL001-70BEZ and EVAL-CN0303_SDPZ =====
   - First, connect the discrete female colored cable to connector P1 of the [[adi>en/mems-sensors/mems-inertial-sensors/adxl001/products/EVAL-ADXL001/eb.html|ADXL001-70BEZ]].   - First, connect the discrete female colored cable to connector P1 of the [[adi>en/mems-sensors/mems-inertial-sensors/adxl001/products/EVAL-ADXL001/eb.html|ADXL001-70BEZ]].
-  - Secondly, connect the discrete female colored cable to connector J6 of the [[adi>eval-cn0303-sdpz|EVAL-CN0303-SDPZ]].{{ :resources:eval:user-guides:circuits-from-the-lab:cn0303:PCB.jpg? |}} +  - Secondly, connect the discrete female colored cable to connector J6 of the EVAL-CN0303-SDPZ.{{ :resources:eval:user-guides:circuits-from-the-lab:cn0303:PCB.jpg? |}} 
-  - Connect the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] and the [[adi>eval-cn0303-sdpz|EVAL-CN0303-SDPZ]] PCB’s using the 120 pin male and female connectors found on the respective boards to **Connector A** of the the SDP-B board. +  - Connect the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] and the EVAL-CN0303-SDPZ PCB’s using the 120 pin male and female connectors found on the respective boards to **Connector A** of the the SDP-B board. 
-  - Plug in the DC barrel jack to connector J5 of the [[adi>eval-cn0303-sdpz|EVAL-CN0303-SDPZ]] and the mini end of the USB cable into connector J1 of the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]]. And connect the other end of the USB cable into the Laptop or PC.+  - Plug in the DC barrel jack to connector J5 of the EVAL-CN0303-SDPZ and the mini end of the USB cable into connector J1 of the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]]. And connect the other end of the USB cable into the Laptop or PC.
 {{ :resources:eval:user-guides:circuits-from-the-lab:cn0303:PCB + Cables.jpg? |}} {{ :resources:eval:user-guides:circuits-from-the-lab:cn0303:PCB + Cables.jpg? |}}
  
Line 59: Line 63:
       - **Clear Data** - This button clears the graph and deletes the array containing the FFT data and any indicators such as 'Max Code', 'Min Code', 'Pk-to-Pk Codes', 'Pk-to-Pk Volts' etc.       - **Clear Data** - This button clears the graph and deletes the array containing the FFT data and any indicators such as 'Max Code', 'Min Code', 'Pk-to-Pk Codes', 'Pk-to-Pk Volts' etc.
 {{ :resources:eval:user-guides:circuits-from-the-lab:cn0303:software_-_frequency_results_tab.png |}} {{ :resources:eval:user-guides:circuits-from-the-lab:cn0303:software_-_frequency_results_tab.png |}}
 +
 +=====Registration===== 
 +<WRAP round tip 80% >
 +Receive software update notifications, documentation updates, view the latest videos, and more when you register your hardware.  [[reg>EVAL-CN0303-SDPZ?&v=RevA|Register]] to receive all these great benefits and more!
 +</WRAP>
resources/eval/user-guides/circuits-from-the-lab/cn0303.txt · Last modified: 29 Jul 2021 07:22 by Harvey John De Chavez