This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0303 [15 Jul 2013 22:33] – [Step by Step Instruction to Using the Evaluation Software] Neil Wilson | resources:eval:user-guides:circuits-from-the-lab:cn0303 [03 Jan 2021 21:55] – fix links Robin Getz | ||
---|---|---|---|
Line 5: | Line 5: | ||
===== General Setup ===== | ===== General Setup ===== | ||
- | *One [[http:// | + | *One [[adi>CN0303|EVAL-CN0303-SDPZ]] Evaluation Board |
- | *One [[http:// | + | *One [[adi>en/ |
- | *[[http:// | + | *[[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Evaluation board |
*[[ftp:// | *[[ftp:// | ||
*One 6V wallwart. | *One 6V wallwart. | ||
Line 38: | Line 38: | ||
{{ : | {{ : | ||
===== Instructions for connecting the ADXL001-70BEZ and EVAL-CN0303_SDPZ ===== | ===== Instructions for connecting the ADXL001-70BEZ and EVAL-CN0303_SDPZ ===== | ||
- | - First, connect the discrete female colored cable to connector P1 of the [[http:// | + | - First, connect the discrete female colored cable to connector P1 of the [[adi>en/ |
- | - Secondly, connect the discrete female colored cable to connector J6 of the [[http:// | + | - Secondly, connect the discrete female colored cable to connector J6 of the [[adi>eval-cn0303-sdpz|EVAL-CN0303-SDPZ]].{{ : |
- | - Connect the [[http:// | + | - Connect the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] and the [[adi>eval-cn0303-sdpz|EVAL-CN0303-SDPZ]] PCB’s using the 120 pin male and female connectors found on the respective boards |
- | - Plug in the DC barrel jack to connector J5 of the [[http:// | + | - Plug in the DC barrel jack to connector J5 of the [[adi>eval-cn0303-sdpz|EVAL-CN0303-SDPZ]] and the mini end of the USB cable into connector J1 of the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]]. And connect the other end of the USB cable into the Laptop or PC. |
{{ : | {{ : | ||
Line 51: | Line 51: | ||
- The following is a list of all available software controls found in the **Acceleration Results** tab, grouped according to their location in the software: | - The following is a list of all available software controls found in the **Acceleration Results** tab, grouped according to their location in the software: | ||
- **System Controls** | - **System Controls** | ||
- | - **Connect** – This button configures the [[http:// | + | - **Connect** – This button configures the [[adi>ad7476|AD7476]] by writing to the necessary registers. |
- **Connector A** - This menu allows the user to select which connector of the SDP board is being utilized. | - **Connector A** - This menu allows the user to select which connector of the SDP board is being utilized. | ||
- **Data Acquisition Controls** | - **Data Acquisition Controls** |