This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0303 [15 Jul 2013 21:32] – [Opening and Enabling the Evaluation Software] Neil Wilson | resources:eval:user-guides:circuits-from-the-lab:cn0303 [08 Feb 2021 18:47] – retire Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | ====== Vibration Analysis (CN0303) ====== | ||
+ | {{page>/ | ||
+ | |||
+ | An [[adi> | ||
+ | |||
+ | ===== Overview ===== | ||
+ | This circuit offers a high linearity, low noise, wide-bandwidth vibration sensing solution. | ||
+ | |||
+ | ===== General Setup ===== | ||
+ | *One EVAL-CN0303-SDPZ Evaluation Board | ||
+ | *One [[adi> | ||
+ | *[[adi> | ||
+ | *CN0303 Evaluation Software | ||
+ | *One 6V wallwart. | ||
+ | *One DC power supply with a 0-6V output. | ||
+ | *One USB Type-A plug to USB Mini-B plug cable. | ||
+ | ===== Minimum PC/System Requirements ===== | ||
+ | * One PC with the following | ||
+ | * Windows XP SP2, Windows Vista or Windows 7 Business/ | ||
+ | * Intel Pentium processor (x86 compatible), | ||
+ | * 512 MB RAM and 2 GB available hard disk space | ||
+ | * .NET 3.5 Framework | ||
+ | |||
+ | ===== How to Install the Evaluation Software ===== | ||
+ | - Extract the files within the file **CN0303 SDP Eval Software.zip** and open the file **setup.exe**. | ||
+ | - Press **“Next”**.{{ : | ||
+ | - Press **“Next”**.{{ : | ||
+ | - Press **“Next”**. | ||
+ | - Upon completion of the installation of the **CN0303 SDP Eval Software**, the installer for the **ADI SDP Drivers** will execute. | ||
+ | - {{ : | ||
+ | - Press **“Next”**. | ||
+ | - {{ : | ||
+ | - It is recommended that you install the drivers to the default directory path **C: | ||
+ | - Press **“Next”** to install the Drivers and complete the installation of all software necessary to evaluate the **EVAL-CN0303-SDPZ** | ||
+ | ===== Step by Step Instruction for Preparing the ADXL001 Evaluation Board ===== | ||
+ | |||
+ | - In order to mitigate high frequency noise outside of the vibration band of interest, a basic RC low pass filter is created by components R1 and C2. | ||
+ | - The recommended cutoff frequency is 80kHz (R1 = 1k, C2 = 1nF). This will remove any high frequency noise above 80kHz. | ||
+ | - The cutoff frequency can be adjusted by manipulating R1 and C2. | ||
+ | - A filter is not required. | ||
+ | {{ : | ||
+ | ===== Instructions for connecting the ADXL001-70BEZ and EVAL-CN0303_SDPZ ===== | ||
+ | - First, connect the discrete female colored cable to connector P1 of the [[adi> | ||
+ | - Secondly, connect the discrete female colored cable to connector J6 of the EVAL-CN0303-SDPZ.{{ : | ||
+ | - Connect the [[adi> | ||
+ | - Plug in the DC barrel jack to connector J5 of the EVAL-CN0303-SDPZ and the mini end of the USB cable into connector J1 of the [[adi> | ||
+ | {{ : | ||
+ | |||
+ | ===== Opening and Enabling the Evaluation Software ===== | ||
+ | - Launch the executable found at **C: | ||
+ | {{ : | ||
+ | |||
+ | ===== Step by Step Instruction to Using the Evaluation Software ===== | ||
+ | - The following is a list of all available software controls found in the **Acceleration Results** tab, grouped according to their location in the software: | ||
+ | - **System Controls** | ||
+ | - **Connect** – This button configures the [[adi> | ||
+ | - **Connector A** - This menu allows the user to select which connector of the SDP board is being utilized. | ||
+ | - **Data Acquisition Controls** | ||
+ | - **Acquire Data Set** - This control gathers a number of samples ' | ||
+ | - **FFT Size** - This control determines the number of samples the FFT uses in its calculations. | ||
+ | - **Save Data** - This button prompts and allows the user to save the FFT data to a text file. | ||
+ | - **Clear Data** - This button clears the graph and deletes the array containing the FFT data and any indicators such as 'Max Code', 'Min Code', ' | ||
+ | {{ : |