This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0295 [28 Jul 2017 08:31] – [Sensor Drive] erbe reyta | resources:eval:user-guides:circuits-from-the-lab:cn0295 [29 Jul 2021 07:17] (current) – Hardware Registration Harvey John De Chavez | ||
---|---|---|---|
Line 11: | Line 11: | ||
===== DEMO REQUIREMENTS ===== | ===== DEMO REQUIREMENTS ===== | ||
- | * [[http:// | + | * [[adi>EVAL-CN0295-EB1Z|EVAL-CN0295-EB1Z]] |
* +7V to +24V power supply or equivalent power supply | * +7V to +24V power supply or equivalent power supply | ||
* Precision power supply | * Precision power supply | ||
Line 34: | Line 34: | ||
- A differential output bridge type sensor should be attached to a 4 channel screw terminal block (J3) labeled with SUPPLYSNS on the PCB. | - A differential output bridge type sensor should be attached to a 4 channel screw terminal block (J3) labeled with SUPPLYSNS on the PCB. | ||
- | - A differential sensor gauge like from [[https:// | + | - A differential sensor gauge like from [[http:// |
<note note> | <note note> | ||
* Vsense is where the analog voltage output of the sensor is being taken for measurement. | * Vsense is where the analog voltage output of the sensor is being taken for measurement. | ||
Line 78: | Line 78: | ||
The output of the system can be measured in two ways, either through direct output current measurement or voltage output through the series resistor. | The output of the system can be measured in two ways, either through direct output current measurement or voltage output through the series resistor. | ||
- | {{ : | + | {{ : |
=== * Voltage Measurement === | === * Voltage Measurement === | ||
* Voltage output measurement is done across a series 250ohms resistor though screw type terminal block (P1). | * Voltage output measurement is done across a series 250ohms resistor though screw type terminal block (P1). | ||
- | <note important> | + | <note important> |
{{ : | {{ : | ||
=== * Current Measurement === | === * Current Measurement === | ||
- | * Current output measurement is done by connecting the positive terminal of the current meter at the system ground loop (negative terminal of J2) and the negative terminal of the meter connected to the negative terminal | + | * Current output measurement is done by connecting the positive terminal of the current meter at one pin of the male header shunt terminal |
<note Note> | <note Note> | ||
- | The system has an onboard resistor load (R7) of 250ohms | + | The system has an onboard resistor load (R14) of 500ohms |
</ | </ | ||
Line 106: | Line 107: | ||
</ | </ | ||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | </ | ||
// End of Document // | // End of Document // |