This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0295 [28 Jul 2017 08:16] – [Current Meter] erbe reyta | resources:eval:user-guides:circuits-from-the-lab:cn0295 [29 Jul 2021 07:17] (current) – Hardware Registration Harvey John De Chavez | ||
---|---|---|---|
Line 11: | Line 11: | ||
===== DEMO REQUIREMENTS ===== | ===== DEMO REQUIREMENTS ===== | ||
- | * [[http:// | + | * [[adi>EVAL-CN0295-EB1Z|EVAL-CN0295-EB1Z]] |
* +7V to +24V power supply or equivalent power supply | * +7V to +24V power supply or equivalent power supply | ||
* Precision power supply | * Precision power supply | ||
Line 34: | Line 34: | ||
- A differential output bridge type sensor should be attached to a 4 channel screw terminal block (J3) labeled with SUPPLYSNS on the PCB. | - A differential output bridge type sensor should be attached to a 4 channel screw terminal block (J3) labeled with SUPPLYSNS on the PCB. | ||
- | - A differential sensor gauge like from [[https:// | + | - A differential sensor gauge like from [[http:// |
<note note> | <note note> | ||
* Vsense is where the analog voltage output of the sensor is being taken for measurement. | * Vsense is where the analog voltage output of the sensor is being taken for measurement. | ||
Line 51: | Line 51: | ||
- A precision voltage source generates the 0 to 100 mV differential input voltage at the in-amp input, which then simulates the sensor output shown in the block diagram for test setup. | - A precision voltage source generates the 0 to 100 mV differential input voltage at the in-amp input, which then simulates the sensor output shown in the block diagram for test setup. | ||
- 3 kΩ at R_bridge simulates the bridge type sensor impedance. | - 3 kΩ at R_bridge simulates the bridge type sensor impedance. | ||
+ | |||
+ | {{ : | ||
+ | |||
<note Note>For lower than 5 kΩ bridge resistance, the drive voltage can be decreased down to 5 V using a buffer configuration by removing resistor R6.</ | <note Note>For lower than 5 kΩ bridge resistance, the drive voltage can be decreased down to 5 V using a buffer configuration by removing resistor R6.</ | ||
+ | |||
+ | |||
+ | |||
+ | |||
==== Sensor Drive ==== | ==== Sensor Drive ==== | ||
- | | + | The circuit |
- | ==== Sensor | + | {{ : |
- | | + | |
+ | |||
+ | === Voltage | ||
+ | * In the voltage drive mode with VDRIVE = 10 V, the supply voltage VLOOP or system supply must be greater than 10.2 V | ||
+ | === Current Drive Configuration === | ||
+ | * In the current drive mode, the supply voltage VLOOP or system supply must be greater than 11.2 V in order to maintain sufficient headroom. | ||
<note Note> | <note Note> | ||
- | * The minimum loop supply voltage is also dependent on the configuration | + | Current drive configuration |
- | * In the voltage | + | |
</ | </ | ||
+ | <note important> | ||
+ | Both for voltage and current drive mode, the minimum loop supply voltage is dependent on the configuration of the drive circuit for the bridge. | ||
+ | </ | ||
+ | |||
+ | ==== Output Measurements ==== | ||
+ | The output of the system can be measured in two ways, either through direct output current measurement or voltage output through the series resistor. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | |||
+ | === * Voltage Measurement === | ||
+ | * Voltage output measurement is done across a series 250ohms resistor though screw type terminal block (P1). | ||
+ | <note important> | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | === * Current Measurement === | ||
+ | * Current output measurement is done by connecting the positive terminal of the current meter at one pin of the male header shunt terminal (J1) and the negative terminal of the meter connected to the other pin of the same male header shunt terminal. | ||
+ | |||
+ | <note Note> | ||
+ | The system has an onboard resistor load (R14) of 500ohms that can be de-soldered to replace with a desired resistor load value | ||
+ | </ | ||
+ | |||
---- | ---- | ||
===== SCHEMATICS, PCB LAYOUT, BILL OF MATERIALS ===== | ===== SCHEMATICS, PCB LAYOUT, BILL OF MATERIALS ===== | ||
Line 73: | Line 107: | ||
</ | </ | ||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | </ | ||
// End of Document // | // End of Document // |