This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0295 [24 Jul 2017 08:48] – [Power Supply] erbe reyta | resources:eval:user-guides:circuits-from-the-lab:cn0295 [29 Jul 2021 07:17] (current) – Hardware Registration Harvey John De Chavez | ||
---|---|---|---|
Line 7: | Line 7: | ||
{{ : | {{ : | ||
+ | {{ : | ||
---- | ---- | ||
- | ===== GENERAL SETUP ===== | + | ===== DEMO REQUIREMENTS |
- | * [[http:// | + | * [[adi>EVAL-CN0295-EB1Z|EVAL-CN0295-EB1Z]] |
* +7V to +24V power supply or equivalent power supply | * +7V to +24V power supply or equivalent power supply | ||
+ | * Precision power supply | ||
* Agilent 3458A or equivalent Current meter | * Agilent 3458A or equivalent Current meter | ||
* Differential Pressure sensor or Equivalent Dual channel DC Signal Source | * Differential Pressure sensor or Equivalent Dual channel DC Signal Source | ||
Line 19: | Line 21: | ||
===== HARDWARE SETUP ===== | ===== HARDWARE SETUP ===== | ||
- | {{ : | + | |
Line 26: | Line 28: | ||
<note important> | <note important> | ||
==== Input Signal ==== | ==== Input Signal ==== | ||
- | | + | |
- | * A differential output bridge type sensor should be attached to a 4 channel screw terminal block (J1) labeled with SUPPLYSNS on the PCB. | + | === Using Actual Sensor |
- | * A differential sensor gauge like from [[https:// | + | {{ : |
- | | + | {{ : |
- | * A dual power supply can be used to generate a common-mode voltage of 2.5 V from Vout1 and a 0 mV to 100 mV differential input voltage | + | |
- | * 3 kΩ at R_bridge simulates the bridge type sensor impedance. | + | - A differential output bridge type sensor should be attached to a 4 channel screw terminal block (J3) labeled with SUPPLYSNS on the PCB. |
+ | | ||
+ | <note note> | ||
+ | | ||
+ | * V/Iforce is the sensor excitation or is being supplied either from current or voltage source. | ||
+ | </ | ||
+ | |||
+ | <note important> | ||
+ | Pin polarity for Vsense and for V/Iforce should be take into consideration | ||
+ | </ | ||
+ | |||
+ | === Using Simulated input sensor | ||
+ | The following configuration can be used to simulate the sensor characteristic for evaluation purposes. | ||
+ | {{ : | ||
+ | |||
+ | - A dual power supply can be used to power up the board from Vout1 and to generate a common-mode voltage of 2.5 V from Vout2 shown in the block diagram for test setup. | ||
+ | - A precision voltage source generates the 0 to 100 mV differential input voltage | ||
+ | | ||
+ | |||
+ | {{ : | ||
<note Note>For lower than 5 kΩ bridge resistance, the drive voltage can be decreased down to 5 V using a buffer configuration by removing resistor R6.</ | <note Note>For lower than 5 kΩ bridge resistance, the drive voltage can be decreased down to 5 V using a buffer configuration by removing resistor R6.</ | ||
- | ==== Current Meter ==== | + | |
- | * The Agilent 3458A or any equivalent current meter can be used to measure the actual loop current output of the evaluation board. | + | |
- | ==== Sensor Drive ==== | + | |
- | * The circuit can be switched to the current | + | |
+ | ==== Sensor Drive ==== | ||
+ | The circuit can be switched to the current | ||
+ | {{ : | ||
+ | |||
+ | |||
+ | === Voltage Drive Configuration === | ||
+ | * In the voltage drive mode with VDRIVE = 10 V, the supply voltage VLOOP or system supply must be greater than 10.2 V | ||
+ | === Current Drive Configuration === | ||
+ | * In the current drive mode, the supply voltage VLOOP or system supply must be greater than 11.2 V in order to maintain sufficient headroom. | ||
<note Note> | <note Note> | ||
- | * The minimum loop supply voltage is also dependent on the configuration | + | Current drive configuration |
- | * In the voltage | + | |
</ | </ | ||
+ | <note important> | ||
+ | Both for voltage and current drive mode, the minimum loop supply voltage is dependent on the configuration of the drive circuit for the bridge. | ||
+ | </ | ||
+ | |||
+ | ==== Output Measurements ==== | ||
+ | The output of the system can be measured in two ways, either through direct output current measurement or voltage output through the series resistor. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | |||
+ | === * Voltage Measurement === | ||
+ | * Voltage output measurement is done across a series 250ohms resistor though screw type terminal block (P1). | ||
+ | <note important> | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | === * Current Measurement === | ||
+ | * Current output measurement is done by connecting the positive terminal of the current meter at one pin of the male header shunt terminal (J1) and the negative terminal of the meter connected to the other pin of the same male header shunt terminal. | ||
+ | |||
+ | <note Note> | ||
+ | The system has an onboard resistor load (R14) of 500ohms that can be de-soldered to replace with a desired resistor load value | ||
+ | </ | ||
+ | |||
---- | ---- | ||
===== SCHEMATICS, PCB LAYOUT, BILL OF MATERIALS ===== | ===== SCHEMATICS, PCB LAYOUT, BILL OF MATERIALS ===== | ||
Line 54: | Line 107: | ||
</ | </ | ||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | </ | ||
// End of Document // | // End of Document // |