This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0295 [09 Jan 2021 00:32] – user interwiki links Robin Getz | resources:eval:user-guides:circuits-from-the-lab:cn0295 [29 Jul 2021 07:17] (current) – Hardware Registration Harvey John De Chavez | ||
---|---|---|---|
Line 34: | Line 34: | ||
- A differential output bridge type sensor should be attached to a 4 channel screw terminal block (J3) labeled with SUPPLYSNS on the PCB. | - A differential output bridge type sensor should be attached to a 4 channel screw terminal block (J3) labeled with SUPPLYSNS on the PCB. | ||
- | - A differential sensor gauge like from [[https:// | + | - A differential sensor gauge like from [[http:// |
<note note> | <note note> | ||
* Vsense is where the analog voltage output of the sensor is being taken for measurement. | * Vsense is where the analog voltage output of the sensor is being taken for measurement. | ||
Line 107: | Line 107: | ||
</ | </ | ||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | </ | ||
// End of Document // | // End of Document // |