Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
resources:eval:user-guides:circuits-from-the-lab:cn0288 [03 Jan 2021 21:56] – fix links Robin Getz | resources:eval:user-guides:circuits-from-the-lab:cn0288 [10 Feb 2021 14:42] – fix links Robin Getz |
---|
* [[adi>EVAL-CN0288-SDPZ|EVAL-CN0288-SDPZ]] Evaluation Board (**CN-0288 Board**) | * [[adi>EVAL-CN0288-SDPZ|EVAL-CN0288-SDPZ]] Evaluation Board (**CN-0288 Board**) |
* [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V Power Supply)** or equivalent | * [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V Power Supply)** or equivalent |
* [[adi>EVAL-CFTL-LVDT|EVAL-CFTL-LVDT]] Linear Variable Differential Transformer (Measurement Specialties, Inc. E-100 Economy Series LVDT) | * [[adi>CN0288|EVAL-CFTL-LVDT]] Linear Variable Differential Transformer (Measurement Specialties, Inc. E-100 Economy Series LVDT) |
* [[ftp://ftp.analog.com/pub/cftl/CN0288/|CN-0288 Evaluation Software]] | * [[ftp://ftp.analog.com/pub/cftl/CN0288/|CN-0288 Evaluation Software]] |
* (supplied with provided CD in kit) | * (supplied with provided CD in kit) |
* The [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V DC Power Supply)** powers the [[adi>EVAL-CN0288-SDPZ|EVAL-CN0288-SDPZ]] **(CN-0288 Board)** via the DC barrel jack | * The [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V DC Power Supply)** powers the [[adi>EVAL-CN0288-SDPZ|EVAL-CN0288-SDPZ]] **(CN-0288 Board)** via the DC barrel jack |
* The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. | * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. |
* The [[adi>EVAL-CFTL-LVDT|EVAL-CFTL-LVDT]] **(LVDT)** connects to the [[adi>EVAL-CN0288-SDPZ|EVAL-CN0288-SDPZ]] **(CN-0288 Board)** via the 6-pin header at **J3**. | * The [[adi>CN0288|EVAL-CFTL-LVDT]] **(LVDT)** connects to the [[adi>EVAL-CN0288-SDPZ|EVAL-CN0288-SDPZ]] **(CN-0288 Board)** via the 6-pin header at **J3**. |
\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0288:cn0288-test_setup.png?nolink&|}} | \\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0288:cn0288-test_setup.png?nolink&|}} |
| |
| |
===== Connecting the Hardware ===== | ===== Connecting the Hardware ===== |
- Connect the [[adi>EVAL-CFTL-LVDT|EVAL-CFTL-LVDT]] **(LVDT)** to **J3** of the [[adi>EVAL-CN0288-SDPZ|EVAL-CN0288-SDPZ]] **(CN-0288 Board)** as depicted below.\\ \\ <WRAP left round tip 50%>**NOTE:** If a different LVDT is used other than the E-100 LVDT from Measurement Specialties, Inc the wiring schematic will be different!</WRAP>\\ \\ \\ \\ \\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0288:cn0288-wiring_table.png?nolink& |}}{{:resources:eval:user-guides:circuits-from-the-lab:cn0288:cn0288-wiring_schematic.png?|nolink}}\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0288:cn0288-hardware.png?600|}}\\ \\ | - Connect the [[adi>CN0288|EVAL-CFTL-LVDT]] **(LVDT)** to **J3** of the [[adi>EVAL-CN0288-SDPZ|EVAL-CN0288-SDPZ]] **(CN-0288 Board)** as depicted below.\\ \\ <WRAP left round tip 50%>**NOTE:** If a different LVDT is used other than the E-100 LVDT from Measurement Specialties, Inc the wiring schematic will be different!</WRAP>\\ \\ \\ \\ \\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0288:cn0288-wiring_table.png?nolink& |}}{{:resources:eval:user-guides:circuits-from-the-lab:cn0288:cn0288-wiring_schematic.png?|nolink}}\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0288:cn0288-hardware.png?600|}}\\ \\ |
- Connect **J8** of the [[adi>EVAL-CN0288-SDPZ|EVAL-CN0288-SDPZ]] **(CN-0288 Board)** to **CON A** of the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)**\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0288:cn0288-hardware2.png?600|}}\\ \\ | - Connect **J8** of the [[adi>EVAL-CN0288-SDPZ|EVAL-CN0288-SDPZ]] **(CN-0288 Board)** to **CON A** of the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)**\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0288:cn0288-hardware2.png?600|}}\\ \\ |
- Connect the [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V DC Power Supply)** to the Barrel Jack at **J4** or the Screw Terminal at **J1** on the [[adi>EVAL-CN0288-SDPZ|EVAL-CN0288-SDPZ]] **(CN-0288 Board)**\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0288:cn0288-hardware3.png?600|}}\\ \\ | - Connect the [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V DC Power Supply)** to the Barrel Jack at **J4** or the Screw Terminal at **J1** on the [[adi>EVAL-CN0288-SDPZ|EVAL-CN0288-SDPZ]] **(CN-0288 Board)**\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0288:cn0288-hardware3.png?600|}}\\ \\ |