This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0276 [27 Sep 2013 05:21] – 0 Robert Lee | resources:eval:user-guides:circuits-from-the-lab:cn0276 [18 Jul 2023 04:59] (current) – Angelo Nikko Catapang | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== CN0276 Software User Guide ====== | + | ====== CN0276 Software User Guide ====== |
===== OVERVIEW ===== | ===== OVERVIEW ===== | ||
- | [[http:// | + | [[adi>CN0276|CN-0276]] is a high performance |
- | The[[http:// | + | In the system AD2S1210 generated programmable excitation signals, the AD8692 and AD8397 compose third order butterworth lowpass filter and power amplifier. |
- | {{ : | + | |
+ | The maximum tracking rate of the RDC is 3125 rps in the 10-bit mode (resolution = 21 arc min) and 156.25 rps in the 16-bit mode (resolution = 19.8 arc sec). | ||
+ | {{ : | ||
+ | ===== Required Equipment ===== | ||
+ | * [[adi> | ||
+ | * [[adi> | ||
+ | * Resolver: [[http:// | ||
+ | * Adjustable DC power supplies, output should be satisfied: from +6V to +12V over than 500mA. | ||
+ | * USB Type-A plug to USB Mini-B plug cable | ||
+ | * PC with the following | ||
+ | * Microsoft Windows 7 with sp1 x86 or x64 version, or later | ||
+ | * Intel Core processor (x86 or x64 compatible), | ||
+ | * At least 4GB RAM and 8GB available hard disk space | ||
+ | * [[http:// | ||
+ | * [[http:// | ||
+ | * SDP EEPROM Programmer software | ||
+ | * Supplied with CD | ||
+ | * CN0276 Programming File | ||
+ | * Supplied with CD | ||
+ | * CN0276 SDP Evaluation Software | ||
+ | * Supplied with CD | ||
+ | ===== General Setup ===== | ||
+ | |||
+ | * The [[adi> | ||
+ | * Use the Adjustable DC power supplies to powers the [[adi> | ||
+ | * The [[adi> | ||
+ | * The [[http:// | ||
+ | |||
+ | |||
+ | {{ : | ||
+ | ---- | ||
+ | ===== Installing the Software ===== | ||
+ | - Extract the file **CN0276_Evaluation_Software.zip** and open the file **setup.exe**.\\ \\ <WRAP left tip round box 60%> | ||
+ | - Click **Next** to view the installation review page\\ \\ {{ : | ||
+ | - Click **Next** to start the installation, | ||
+ | - Press **“Next”** to set the installation location for the **SDP Drivers**.\\ \\ <WRAP left round tip 50%>It is recommended that you install the drivers to the default directory path \\ **C: | ||
+ | - Press **“Next”** to install the **SDP Drivers** and complete the installation of all software. | ||
+ | |||
+ | ---- | ||
+ | ===== Connecting the Hardware ===== | ||
+ | * Connect the [[http:// | ||
+ | |||
+ | ^ J3 Pins ^ Signals ^ TS2620N21E11 wire ^ | ||
+ | |1 |COS |Red | | ||
+ | |2 |COSLO |Black | | ||
+ | |3 |SINLO |Blue | | ||
+ | |4 |SIN |Yellow | | ||
+ | |5 |EXC |Red/White | | ||
+ | |6 |nEXC |Yellow/ | ||
+ | |||
+ | * Connect the adjustable DC power supplies to the **J4** of the [[adi> | ||
+ | |||
+ | ^ J4 Pins ^ Types ^ | ||
+ | |1 |VCC | | ||
+ | |2 |GND | | ||
+ | |||
+ | ---- | ||
+ | |||
+ | ===== Using the Evaluation Software ===== | ||
+ | ==== Software Control and Indicator Descriptions ==== | ||
+ | {{ : | ||
+ | {{ : | ||
+ | {{ : | ||
+ | -**Connect/ | ||
+ | * When this button is clicked, the SDP-B Board USB connection to the CN-0276 Board status will be filliped. | ||
+ | -**Start Button** | ||
+ | * When this button is pressed, the SDP-B Board will collect conversion data and present the acquisitions in the chart. | ||
+ | -**Stop Button** | ||
+ | * When this button is pressed, the software stop collecting data from the CN-0276 Board. | ||
+ | -**Samples setting** | ||
+ | * The number which input to this box is use to set the samples for each time the start button pressed. | ||
+ | -**Run mode setting** | ||
+ | * The check box set the persistent running mode of RDC samples. | ||
+ | -**Control Tabs** | ||
+ | * __Data Analyze__ This Tab showing the acquired data analyzed result in histogram. | ||
+ | * __RDC Output__ This Tab include two indicators to showing the position and velocity output of RDC, update in real time when RDC is converting. | ||
+ | * __RDC Configuration__ This Tab use to write and read the internal register of AD2S1210 | ||
+ | * __SDP Information__ Showing the SDP-B Board information when USB connection available. | ||
+ | -**SDP Status String Indicator** | ||
+ | * This indicator displays a message to the SDP-B Board. | ||
+ | -**RDC working Status LED** | ||
+ | * This LED showing the RDC working status, when RDC is converting this LED will be light up, otherwise it will be turn off. | ||
+ | -**Position indicator** | ||
+ | * This indicator display the RDC position output in hexadecimal. | ||
+ | -**Velocity indicator** | ||
+ | * This indicator display the RDC velocity output in rps(revolutions per second). | ||
+ | -**Configuration write to AD2S1210** | ||
+ | * These values will be write to the AD2S1210' | ||
+ | -**AD2S1210 register value** | ||
+ | * These values is the read back of the AD2S1210' | ||
+ | -**AD2S1210 Fault LED** | ||
+ | * These LED showing the fault status of AD2S1210. | ||
+ | -**Write Configuration Button** | ||
+ | * When this button is pressed, the values on the configuration area will write to the AD2S1210' | ||
+ | |||
+ | ---- | ||
+ | ==== Establishing a USB Connection Link ==== | ||
+ | - Follow the instructions to properly install the software and connect the hardware as described in the previous sections. | ||
+ | - Open the file named **CN0276.exe** in the installation directory.\\ \\ <WRAP left info round box 60%> | ||
+ | - Click the **Connect Button**. | ||
+ | - Upon success, the **System Status String Indicator** will display __SDP Board serial number__ | ||
+ | |||
+ | ---- | ||
+ | ==== Capturing Data ==== | ||
+ | - **Establish a USB Connection Link**. | ||
+ | - **Write the configure data to AD2S1210**.\\ \\ <WRAP important> | ||
+ | - **Setting the sample times**. | ||
+ | - Click the **Start Button**. | ||
+ | - when sample times reached the sample times setting or **Stop Button** has been pressed, the converting will be halt. | ||
+ | |||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | </ |