Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:circuits-from-the-lab:cn0274 [03 Jan 2021 21:55] – fix links Robin Getz | resources:eval:user-guides:circuits-from-the-lab:cn0274 [29 Jul 2021 06:06] (current) – Hardware Registration Harvey John De Chavez |
---|
===== General Setup ===== | ===== General Setup ===== |
* [[adi>EVAL-CN0274-SDPZ|EVAL-CN0274-SDPZ]] Evaluation board. | * [[adi>EVAL-CN0274-SDPZ|EVAL-CN0274-SDPZ]] Evaluation board. |
* [[adi>EVAL-SDP-CS1Z|EVAL-SDP-CS1Z]] Evaluation board | * [[adi>SDP-S|EVAL-SDP-CS1Z]] Evaluation board |
* [[ftp://ftp.analog.com/pub/cftl/CN0274|CN0274 Evaluation Software]] | * [[ftp://ftp.analog.com/pub/cftl/CN0274|CN0274 Evaluation Software]] |
* Power Supply: 2 AAA batteries or +3.0V supply. | * Power Supply: 2 AAA batteries or +3.0V supply. |
===== Step by Step Instruction for Connecting the Hardware ===== | ===== Step by Step Instruction for Connecting the Hardware ===== |
- Place two batteries into the connector on the bottom of the [[adi>eval-cn0274-sdpz|EVAL-CN0274-SDPZ]] board, ensure the batteries are size triple A and are the correct polarity.{{:resources:eval:user-guides:circuits-from-the-lab:cn0274:cn0274-hardware-batteries.jpg?200|}}{{:resources:eval:user-guides:circuits-from-the-lab:cn0274:cn0274-hardware-cn0274.jpg?200|}} | - Place two batteries into the connector on the bottom of the [[adi>eval-cn0274-sdpz|EVAL-CN0274-SDPZ]] board, ensure the batteries are size triple A and are the correct polarity.{{:resources:eval:user-guides:circuits-from-the-lab:cn0274:cn0274-hardware-batteries.jpg?200|}}{{:resources:eval:user-guides:circuits-from-the-lab:cn0274:cn0274-hardware-cn0274.jpg?200|}} |
- Connect the [[adi>EVAL-SDP-CS1Z|EVAL-SDP-CS1Z]] and the [[adi>eval-cn0274-sdpz|EVAL-CN0274-SDPZ]] PCB’s using the 120 pin male and female connectors found on the respective boards.{{:resources:eval:user-guides:circuits-from-the-lab:cn0274:cn0274-hardware-notconnected-sdps-cn0274.jpg?200|}}{{:resources:eval:user-guides:circuits-from-the-lab:cn0274:cn0274-hardware-displaying_connectors.jpg?200|}}{{:resources:eval:user-guides:circuits-from-the-lab:cn0274:cn0274-hardware-connectorscloseup.jpg?200|}}{{:resources:eval:user-guides:circuits-from-the-lab:cn0274:cn0274-hardware-connected-sdps-cn0274.jpg?200|}} | - Connect the [[adi>SDP-S|EVAL-SDP-CS1Z]] and the [[adi>eval-cn0274-sdpz|EVAL-CN0274-SDPZ]] PCB’s using the 120 pin male and female connectors found on the respective boards.{{:resources:eval:user-guides:circuits-from-the-lab:cn0274:cn0274-hardware-notconnected-sdps-cn0274.jpg?200|}}{{:resources:eval:user-guides:circuits-from-the-lab:cn0274:cn0274-hardware-displaying_connectors.jpg?200|}}{{:resources:eval:user-guides:circuits-from-the-lab:cn0274:cn0274-hardware-connectorscloseup.jpg?200|}}{{:resources:eval:user-guides:circuits-from-the-lab:cn0274:cn0274-hardware-connected-sdps-cn0274.jpg?200|}} |
- Plug the mini end of the USB cable into connector J2 of the [[adi>EVAL-SDP-CS1Z|EVAL-SDP-CS1Z]]. And connect the other end of the USB cable into the Laptop or PC.{{:resources:eval:user-guides:circuits-from-the-lab:cn0274:cn0274-hardware-connected-usb-sdps-cn0274.jpg?200|}} | - Plug the mini end of the USB cable into connector J2 of the [[adi>SDP-S|EVAL-SDP-CS1Z]]. And connect the other end of the USB cable into the Laptop or PC.{{:resources:eval:user-guides:circuits-from-the-lab:cn0274:cn0274-hardware-connected-usb-sdps-cn0274.jpg?200|}} |
===== Opening and Enabling the Evaluation Software ===== | ===== Opening and Enabling the Evaluation Software ===== |
- Launch the executable found at **C:\Program Files\Analog Devices\CN0274** and press the **“Connect"** button.{{ :resources:eval:user-guides:circuits-from-the-lab:cn0274:cn0274-evaluation_software-front_panel.jpg? |}} | - Launch the executable found at **C:\Program Files\Analog Devices\CN0274** and press the **“Connect"** button.{{ :resources:eval:user-guides:circuits-from-the-lab:cn0274:cn0274-evaluation_software-front_panel.jpg? |}} |
- **System Controls** | - **System Controls** |
- **Connect** – This button configures the [[adi>adxl362|ADXL362]] by writing to the necessary registers. A prompt will appear informing the user if the accelerometer was properly configured. | - **Connect** – This button configures the [[adi>adxl362|ADXL362]] by writing to the necessary registers. A prompt will appear informing the user if the accelerometer was properly configured. |
- **Disconnect** – This button will disconnect the [[http://analog.com/eval-cn0274-sdpz|EVAL-CN0274-SDPZ]] board. | - **Disconnect** – This button will disconnect the [[adi>eval-cn0274-sdpz|EVAL-CN0274-SDPZ]] board. |
- **Data Acquisition Controls** | - **Data Acquisition Controls** |
- **Start Sampling** – This button polls the data ready bit in the [[adi>adxl362|ADXL362]] status register. When this bit is set, LabVIEW reads the data registers and displays the acceleration data for each axis on the chart found in the evaluation software. | - **Start Sampling** – This button polls the data ready bit in the [[adi>adxl362|ADXL362]] status register. When this bit is set, LabVIEW reads the data registers and displays the acceleration data for each axis on the chart found in the evaluation software. |
- Z-Axis Plot Disabled/Enabled- This control disables or enables the graphical display for the Z-axis. | - Z-Axis Plot Disabled/Enabled- This control disables or enables the graphical display for the Z-axis. |
| |
| =====Registration===== |
| <WRAP round tip 80% > |
| Receive software update notifications, documentation updates, view the latest videos, and more when you register your hardware. [[reg>EVAL-CN0274-SDPZ?&v=RevA|Register]] to receive all these great benefits and more! |
| </WRAP> |