Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
resources:eval:user-guides:circuits-from-the-lab:cn0274 [17 Sep 2012 23:35] – [Opening and Enabling the Evaluation Software] Neil Wilson | resources:eval:user-guides:circuits-from-the-lab:cn0274 [29 Nov 2012 18:51] – [Opening and Enabling the Evaluation Software] James Fitzgerald |
---|
* Power Supply: 2 AAA batteries or +3.0V supply. | * Power Supply: 2 AAA batteries or +3.0V supply. |
* 1 USB Type-A plug to USB Mini-B plug cable | * 1 USB Type-A plug to USB Mini-B plug cable |
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0274-setupdiagram.jpg? |}} | {{ :resources:eval:user-guides:circuits-from-the-lab:cn0274:cn0274-setupdiagram.jpg? |}} |
| |
===== Minimum PC/System Requirements ===== | ===== Minimum PC/System Requirements ===== |
| |
===== How to Install the Evaluation Software ===== | ===== How to Install the Evaluation Software ===== |
- Extract the files within the file **CN0274 SDP Eval Software.zip** and open the file **setup.exe**. It is recommended that you install the CN0274 SDP Evaluation Software to the default directory path **C:\Program Files\Analog Devices\CN0274\** and all National Instruments products to **C:\Program Files\National Instruments\**{{ :resources:eval:user-guides:circuits-from-the-lab:cn0274-evaluation_software-destination_directory-1.jpg? |}} | - Extract the files within the file **CN0274 SDP Eval Software.zip** and open the file **setup.exe**. It is recommended that you install the CN0274 SDP Evaluation Software to the default directory path **C:\Program Files\Analog Devices\CN0274\** and all National Instruments products to **C:\Program Files\National Instruments\**{{ :resources:eval:user-guides:circuits-from-the-lab:cn0274:cn0274-evaluation_software-destination_directory-1.jpg? |}} |
- Press **“Next”**.{{ :resources:eval:user-guides:circuits-from-the-lab:cn0274-evaluation_software-destination_directory-2.jpg? |}} | - Press **“Next”**.{{ :resources:eval:user-guides:circuits-from-the-lab:cn0274:cn0274-evaluation_software-destination_directory-2.jpg? |}} |
- Press **“Next”**.{{ :resources:eval:user-guides:circuits-from-the-lab:cn0274-evaluation_software-installation_complete.jpg? |}} | - Press **“Next”**.{{ :resources:eval:user-guides:circuits-from-the-lab:cn0274:cn0274-evaluation_software-installation_complete.jpg? |}} |
- Press **“Next”**. | - Press **“Next”**. |
- Upon completion of the installation of the **CN0274 SDP Eval Software**, the installer for the **ADI SDP Drivers** will execute. Follow the on-screen prompts to install the drivers. It is recommended that you close all other applications before clicking “Next”. This will make it possible to update relevant system files without having to reboot your computer.{{ :resources:eval:user-guides:circuits-from-the-lab:cn0274-sdpdrivers-setup_wizard.jpg? |}}{{ :resources:eval:user-guides:circuits-from-the-lab:cn0274-sdpdrivers-destination_directory.jpg? |}} | - Upon completion of the installation of the **CN0274 SDP Eval Software**, the installer for the **ADI SDP Drivers** will execute. Follow the on-screen prompts to install the drivers. It is recommended that you close all other applications before clicking “Next”. This will make it possible to update relevant system files without having to reboot your computer.{{ :resources:eval:user-guides:circuits-from-the-lab:cn0274:cn0274-sdpdrivers-setup_wizard.jpg? |}}{{ :resources:eval:user-guides:circuits-from-the-lab:cn0274:cn0274-sdpdrivers-destination_directory.jpg? |}} |
- Press **“Next”**. | - Press **“Next”**. |
- It is recommended that you install the drivers to the default directory path **C:\Program Files\Analog Devices\SDP\Drivers\** | - It is recommended that you install the drivers to the default directory path **C:\Program Files\Analog Devices\SDP\Drivers\** |
- Press **“Next”** to install the Drivers and complete the installation of all software necessary to evaluate the **EVAL-CN0274-SDPZ** | - Press **“Next”** to install the Drivers and complete the installation of all software necessary to evaluate the **EVAL-CN0274-SDPZ** |
| |
===== Step by Step Instruction for Connecting the Hardware ===== | ===== Step by Step Instruction for Connecting the Hardware ===== |
- Place two batteries into the connector on the bottom of the [[http://www.analog.com/eval-cn0274-sdpz|EVAL-CN0274-SDPZ]] board, ensure the batteries are size triple A and are the correct polarity.{{:resources:eval:user-guides:circuits-from-the-lab:cn0274-hardware-batteries.jpg?200|}}{{:resources:eval:user-guides:circuits-from-the-lab:cn0274-hardware-cn0274.jpg?200|}} | - Place two batteries into the connector on the bottom of the [[http://www.analog.com/eval-cn0274-sdpz|EVAL-CN0274-SDPZ]] board, ensure the batteries are size triple A and are the correct polarity.{{:resources:eval:user-guides:circuits-from-the-lab:cn0274:cn0274-hardware-batteries.jpg?200|}}{{:resources:eval:user-guides:circuits-from-the-lab:cn0274:cn0274-hardware-cn0274.jpg?200|}} |
- Connect the [[http://www.analog.com/EVAL-SDP-CS1Z|EVAL-SDP-CS1Z]] and the [[http://www.analog.com/eval-cn0274-sdpz|EVAL-CN0274-SDPZ]] PCB’s using the 120 pin male and female connectors found on the respective boards.{{:resources:eval:user-guides:circuits-from-the-lab:cn0274-hardware-notconnected-sdps-cn0274.jpg?200|}}{{:resources:eval:user-guides:circuits-from-the-lab:cn0274-hardware-displaying_connectors.jpg?200|}}{{:resources:eval:user-guides:circuits-from-the-lab:cn0274-hardware-connectorscloseup.jpg?200|}}{{:resources:eval:user-guides:circuits-from-the-lab:cn0274-hardware-connected-sdps-cn0274.jpg?200|}} | - Connect the [[http://www.analog.com/EVAL-SDP-CS1Z|EVAL-SDP-CS1Z]] and the [[http://www.analog.com/eval-cn0274-sdpz|EVAL-CN0274-SDPZ]] PCB’s using the 120 pin male and female connectors found on the respective boards.{{:resources:eval:user-guides:circuits-from-the-lab:cn0274:cn0274-hardware-notconnected-sdps-cn0274.jpg?200|}}{{:resources:eval:user-guides:circuits-from-the-lab:cn0274:cn0274-hardware-displaying_connectors.jpg?200|}}{{:resources:eval:user-guides:circuits-from-the-lab:cn0274:cn0274-hardware-connectorscloseup.jpg?200|}}{{:resources:eval:user-guides:circuits-from-the-lab:cn0274:cn0274-hardware-connected-sdps-cn0274.jpg?200|}} |
- Plug the mini end of the USB cable into connector J2 of the [[http://www.analog.com/EVAL-SDP-CS1Z|EVAL-SDP-CS1Z]]. And connect the other end of the USB cable into the Laptop or PC.{{:resources:eval:user-guides:circuits-from-the-lab:cn0274-hardware-connected-usb-sdps-cn0274.jpg?200|}} | - Plug the mini end of the USB cable into connector J2 of the [[http://www.analog.com/EVAL-SDP-CS1Z|EVAL-SDP-CS1Z]]. And connect the other end of the USB cable into the Laptop or PC.{{:resources:eval:user-guides:circuits-from-the-lab:cn0274:cn0274-hardware-connected-usb-sdps-cn0274.jpg?200|}} |
===== Opening and Enabling the Evaluation Software ===== | ===== Opening and Enabling the Evaluation Software ===== |
- Launch the executable found at **C:\Program Files\Analog Devices\CN0274** and press the **“Connect"** button.{{ :resources:eval:user-guides:circuits-from-the-lab:cn0274-evaluation_software-front_panel.jpg? |}} | - Launch the executable found at **C:\Program Files\Analog Devices\CN0274** and press the **“Connect"** button.{{ :resources:eval:user-guides:circuits-from-the-lab:cn0274:cn0274-evaluation_software-front_panel.jpg? |}} |
- After pressing the **“Connect”** button, a prompt will appear informing the user if the accelerometer was properly configured. Press **“Ok”** and the software is ready to use. If the accelerometer is not configured properly, disconnect the entire setup and start over. | - After pressing the **“Connect”** button, a prompt will appear informing the user if the accelerometer was properly configured. Press **“Ok”** and the software is ready to use. If the accelerometer is not configured properly, disconnect the entire setup and start over. |
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0274-evaluation_software-accelerometer_configuration_successful.jpg? |}} | {{ :resources:eval:user-guides:circuits-from-the-lab:cn0274:cn0274-evaluation_software-accelerometer_configuration_successful.jpg? |}} |
===== Step by Step Instruction to Using the Evaluation Software ===== | ===== Step by Step Instruction to Using the Evaluation Software ===== |
- The following is a list of all available software controls, grouped according to their location in the software: | - The following is a list of all available software controls, grouped according to their location in the software: |