Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0269 [15 Oct 2013 11:32] – [Capturing a Single Capture] yue huaresources:eval:user-guides:circuits-from-the-lab:cn0269 [29 Jul 2021 05:56] (current) – Hardware Registration Harvey John De Chavez
Line 1: Line 1:
- 
-} 
 ====== CN-0269 Software User Guide ====== ====== CN-0269 Software User Guide ======
 +
 ===== Overview ===== ===== Overview =====
-[[http://www.analog.com/CN0287|CN-0269]] is a high performance industrial signal level multi-channel data acquisition circuit that can process 16-channels of single-ended inputs or 8-channels of differential inputs with up to 18-bit resolution.+[[adi>CN0287|CN-0269]] is a high performance industrial signal level multi-channel data acquisition circuit that can process 16-channels of single-ended inputs or 8-channels of differential inputs with up to 18-bit resolution.
  
 A single channel can be sampled at up to 1.33 MSPS with 18-bit resolution. A channel-to-channel switching rate of 250 kHz between all input channels provides 16-bit performance. A single channel can be sampled at up to 1.33 MSPS with 18-bit resolution. A channel-to-channel switching rate of 250 kHz between all input channels provides 16-bit performance.
Line 11: Line 10:
 \\ {{ :resources:eval:user-guides:circuits-from-the-lab:cn0269:cn0269-symlified-schematic.png?direct&900 |}} \\ {{ :resources:eval:user-guides:circuits-from-the-lab:cn0269:cn0269-symlified-schematic.png?direct&900 |}}
 ===== Required Equipment ===== ===== Required Equipment =====
-  * [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Evaluation Board (**SDP-B Board**) +  * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Evaluation Board (**SDP-B Board**) 
-  * [[http://www.analog.com/EVAL-CN0269-SDPZ|EVAL-CN0269-SDPZ]] Daughter Board (**CN0269 Board**) +  * [[adi>EVAL-CN0269-SDPZ|EVAL-CN0269-SDPZ]] Daughter Board (**CN0269 Board**) 
-  * [[http://www.analog.com/EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] Power Supply or equivalent +6V power supply+  * [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] Power Supply or equivalent +6V power supply
   * [[ftp://ftp.analog.com/pub/cftl/CN0269/|CN0269 SDP Evaluation Software]]   * [[ftp://ftp.analog.com/pub/cftl/CN0269/|CN0269 SDP Evaluation Software]]
     * (supplied with provided CD in kit)     * (supplied with provided CD in kit)
Line 24: Line 23:
   * Signal Generator for Sin Wave with +/-10V Vpp and frequency upto 500KHz   * Signal Generator for Sin Wave with +/-10V Vpp and frequency upto 500KHz
 ===== General Setup ===== ===== General Setup =====
-  * The **[[http://www.analog.com/EVAL-CN0269-SDPZ|EVAL-CN0269-SDPZ]]** Board connects to the **[[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]]** SDP-B Board via the 120-Pin connector +  * The **[[adi>EVAL-CN0269-SDPZ|EVAL-CN0269-SDPZ]]** Board connects to the **[[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]]** SDP-B Board via the 120-Pin connector 
-  * The DC Power Supply +6V Output connects to **CN2** on **[[http://www.analog.com/EVAL-CN0269-SDPZ|EVAL-CN0269-SDPZ]]**, The DC Power Supply +/-12V connects to **CN1** on the **[[http://www.analog.com/EVAL-CN0269-SDPZ|EVAL-CN0269-SDPZ]]**. +  * The DC Power Supply +6V Output connects to **CN2** on **[[adi>EVAL-CN0269-SDPZ|EVAL-CN0269-SDPZ]]**, The DC Power Supply +/-12V connects to **CN1** on the **[[adi>EVAL-CN0269-SDPZ|EVAL-CN0269-SDPZ]]**. 
-  * The **[[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]]** SDP-B Board connects to the PC via the USB cable.\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0269:cn0287_test_setup.png?direct&400|}}\\ +  * The **[[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]]** SDP-B Board connects to the PC via the USB cable.\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0269:cn0287_test_setup.png?direct&400|}}\\ 
  
 ===== Installing the Software ===== ===== Installing the Software =====
Line 39: Line 38:
 ===== Connecting the Hardware ===== ===== Connecting the Hardware =====
  
-  - Connect **J1** of the [[http://www.analog.com/EVAL-CN0269-SDPZ|EVAL-CN0269-SDPZ]] (CN0269 Board) to **CON A** of the [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] (SDP-B Board)\\  +  - Connect **J1** of the [[adi>EVAL-CN0269-SDPZ|EVAL-CN0269-SDPZ]] (CN0269 Board) to **CON A** of the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] (SDP-B Board)\\  
-  - Set the JP3 and JP4 on [[http://www.analog.com/EVAL-CN0269-SDPZ|EVAL-CN0269-SDPZ]] (CN0269 Board) to select the input range and Connect the signal correctly according to the pin definition.\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0269:signal_connection_1.png?direct&800|}}\\ \\ +  - Set the JP3 and JP4 on [[adi>EVAL-CN0269-SDPZ|EVAL-CN0269-SDPZ]] (CN0269 Board) to select the input range and Connect the signal correctly according to the pin definition.\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0269:signal_connection_1.png?direct&800|}}\\ \\ 
   - Connect the USB Cable to the SDP-B Board and leave the other side of the cable unconnected.   - Connect the USB Cable to the SDP-B Board and leave the other side of the cable unconnected.
   - Connect the 6V DC power to CN2 and +/-12V DC power to CN1 and Turn on the DC power supply to power up the board.   - Connect the 6V DC power to CN2 and +/-12V DC power to CN1 and Turn on the DC power supply to power up the board.
Line 54: Line 53:
       * When this button is pressed, the SDP-B Board makes a USB connection to the CN0272 Board. A connection to the SDP-B Board must be made to use the software.       * When this button is pressed, the SDP-B Board makes a USB connection to the CN0272 Board. A connection to the SDP-B Board must be made to use the software.
   - **Start Acquisition Button**   - **Start Acquisition Button**
-      * When this button is pressed, the SDP-B Board starts to acquire data from **[[http://www.analog.com/CN0269|EVAL-CN0269-SDPZ]]** Board.+      * When this button is pressed, the SDP-B Board starts to acquire data from **[[adi>CN0269|EVAL-CN0269-SDPZ]]** Board.
   - **Save Data Button**   - **Save Data Button**
       * When this button is pressed, the SDP-B Board save the data into the same directory where the application is installed.\\ \\ <WRAP left round important box 50%>**NOTE:** If the CN0269 SDP Evaluation Software is installed in the default directory, the data files could be found in **C:\Program files\Analog Devices\CN0269\**.</WRAP>\\ \\ \\ \\ \\ \\        * When this button is pressed, the SDP-B Board save the data into the same directory where the application is installed.\\ \\ <WRAP left round important box 50%>**NOTE:** If the CN0269 SDP Evaluation Software is installed in the default directory, the data files could be found in **C:\Program files\Analog Devices\CN0269\**.</WRAP>\\ \\ \\ \\ \\ \\ 
   - **Control Tabs**   - **Control Tabs**
-      * __Configuration Tab__: All the configuration items through [[http://www.analog.com/en/system-demonstration-platform/controller-boards/evaluation/SDP-B/eb.html|EVAL-SDP-CB1Z]] Board to [[http://www.analog.com/CN0269|EVAL-CN0269-SDPZ]] board are organized on this tab. More details about **Configuration Tab** will be introduced in the following Section.+      * __Configuration Tab__: All the configuration items through [[adi>en/system-demonstration-platform/controller-boards/evaluation/SDP-B/eb.html|EVAL-SDP-CB1Z]] Board to [[adi>CN0269|EVAL-CN0269-SDPZ]] board are organized on this tab. More details about **Configuration Tab** will be introduced in the following Section.
       * __Multi-Channel Tab__: This tab shows all the signals on one tab which is convenient to compare the signals from different channels. More details about **Multi-Channel Tab** will be introduced in the following Section.       * __Multi-Channel Tab__: This tab shows all the signals on one tab which is convenient to compare the signals from different channels. More details about **Multi-Channel Tab** will be introduced in the following Section.
       * __Single Channel Tab__: This tab shows the specific channel which is more clearer than Multi-Channel Tab. More details about **Single Channel Tab** will be introduced in the following Section.       * __Single Channel Tab__: This tab shows the specific channel which is more clearer than Multi-Channel Tab. More details about **Single Channel Tab** will be introduced in the following Section.
-      * __SDP Information__: The Firmware version of [[http://www.analog.com/en/system-demonstration-platform/controller-boards/evaluation/SDP-B/eb.html|EVAL-SDP-CB1Z]] Board is shown on this tab. \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0269:sw_info.png?direct&300|}}+      * __SDP Information__: The Firmware version of [[adi>en/system-demonstration-platform/controller-boards/evaluation/SDP-B/eb.html|EVAL-SDP-CB1Z]] Board is shown on this tab. \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0269:sw_info.png?direct&300|}}
   - **Configuration Items**   - **Configuration Items**
-      * All the items that used to control **[[http://www.analog.com/CN0269|EVAL-CN0269-SDPZ]]** board.+      * All the items that used to control **[[adi>CN0269|EVAL-CN0269-SDPZ]]** board.
   - **Hardware Configuration Diagram**   - **Hardware Configuration Diagram**
       * This picture block shows the way of hardware configuration in terms of jumper setting and signal connection according to the current configuration.       * This picture block shows the way of hardware configuration in terms of jumper setting and signal connection according to the current configuration.
Line 76: Line 75:
       * The options are “Connector A” or “Connector B”. The connector to be used must be selected before clicking the **Connect Button**.       * The options are “Connector A” or “Connector B”. The connector to be used must be selected before clicking the **Connect Button**.
     * __**Signal Range Dropdown Menu**__     * __**Signal Range Dropdown Menu**__
-      * This control will select acceptable input range of **[[http://www.analog.com/CN0269|EVAL-CN0269-SDPZ]]** board. After selecting the input range, customer need to make the hardware configuration according the way shown in the **Hardware Configuration Diagram**.+      * This control will select acceptable input range of **[[adi>CN0269|EVAL-CN0269-SDPZ]]** board. After selecting the input range, customer need to make the hardware configuration according the way shown in the **Hardware Configuration Diagram**.
       * The options are -10V to +10V or -5V to +5V.       * The options are -10V to +10V or -5V to +5V.
     * __**Signal Type Dropdown Menu**__     * __**Signal Type Dropdown Menu**__
-      * //8 Channels, Differential//: When this option is selected, **[[http://www.analog.com/CN0269|EVAL-CN0269-SDPZ]]** board could acquire 8-channel differential signals. Pay attention the signal definition under this configuration is different with 16-channel single-ended inputs.  +      * //8 Channels, Differential//: When this option is selected, **[[adi>CN0269|EVAL-CN0269-SDPZ]]** board could acquire 8-channel differential signals. Pay attention the signal definition under this configuration is different with 16-channel single-ended inputs.  
-      * //16 Channels, Single-Ended//: When this option is selected, **[[http://www.analog.com/CN0269|EVAL-CN0269-SDPZ]]** board could acquire 16-channel single-ended signals. Pay attention the signal definition under this configuration is different with 8-channel differential inputs.+      * //16 Channels, Single-Ended//: When this option is selected, **[[adi>CN0269|EVAL-CN0269-SDPZ]]** board could acquire 16-channel single-ended signals. Pay attention the signal definition under this configuration is different with 8-channel differential inputs.
     * __**Acquisition Mode Dropdown Menu**__     * __**Acquisition Mode Dropdown Menu**__
-      * //Single Channel//: When this mode is selected, the Evaluation Software would control **[[http://www.analog.com/en/system-demonstration-platform/controller-boards/evaluation/SDP-B/eb.html|EVAL-SDP-CB1Z]]** Board to collect data from specific channel customer selected. The acquisition rate under **Single Channel Mode** could be up to 1MHz SPS. +      * //Single Channel//: When this mode is selected, the Evaluation Software would control **[[adi>en/system-demonstration-platform/controller-boards/evaluation/SDP-B/eb.html|EVAL-SDP-CB1Z]]** Board to collect data from specific channel customer selected. The acquisition rate under **Single Channel Mode** could be up to 1MHz SPS. 
-      * //All Channel Scan//: When this mode is selected, the Evaluation Software would control **[[http://www.analog.com/en/system-demonstration-platform/controller-boards/evaluation/SDP-B/eb.html|EVAL-SDP-CB1Z]]** Board to collect data from all the channels.(8 Channels for differential input signal and 16 channels for single-ended input signal).+      * //All Channel Scan//: When this mode is selected, the Evaluation Software would control **[[adi>en/system-demonstration-platform/controller-boards/evaluation/SDP-B/eb.html|EVAL-SDP-CB1Z]]** Board to collect data from all the channels.(8 Channels for differential input signal and 16 channels for single-ended input signal).
     * __**Select the Channel Dropdown Menu**__     * __**Select the Channel Dropdown Menu**__
       * This control is shown on the **configuration tab** only when the **Acquisition Mode** is "Single Channel".       * This control is shown on the **configuration tab** only when the **Acquisition Mode** is "Single Channel".
Line 128: Line 127:
     * This Sub Tab shows the distribution status in time domain for the selected channel.     * This Sub Tab shows the distribution status in time domain for the selected channel.
   - **Dynamic Performance Analysis**   - **Dynamic Performance Analysis**
-    * SNR: Signal to Noise Ratio.+    * SNR: Usually, the SNR is the ratio of the rms value of the actual input signal to the rms sum of all other spectral components below the Nyquist frequency, excluding harmonics and dc. The value for SNR is expressed in decibels. (Here the SNR in CN0269 Evaluation Software is used to characterize the dynamic **performance of ADC given the input signal covering all the dynamic range of it**. So, the amplitude of fundamental frequency is equal to 1).
     * SINAD: Signal-to-Noise-and-Distortion Ratio.     * SINAD: Signal-to-Noise-and-Distortion Ratio.
     * SFDR: Spurious Free Dynamic Range.     * SFDR: Spurious Free Dynamic Range.
     * THD: Total Harmonic Distortion.     * THD: Total Harmonic Distortion.
-    * Sin/N: ???+    * Sin/N: The "SNR" to the actual input signal. the ratio of the rms value of the actual input signal to the rms sum of all other spectral components below the Nyquist frequency, excluding harmonics and dc.
     * Fund ampl: Fundamental Frequency Amplitude.     * Fund ampl: Fundamental Frequency Amplitude.
  
Line 156: Line 155:
   - Click the **Start Acquisition**.   - Click the **Start Acquisition**.
  
 +=====Registration=====  
 +<WRAP round tip 80% > 
 +Receive software update notifications, documentation updates, view the latest videos, and more when you register your hardware.  [[reg>EVAL-CN0269-SDPZ?&v=RevA|Register]] to receive all these great benefits and more! 
 +</WRAP>
  
resources/eval/user-guides/circuits-from-the-lab/cn0269.txt · Last modified: 29 Jul 2021 05:56 by Harvey John De Chavez