This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0264 [15 Nov 2017 04:35] – update Trisha Cabildo | resources:eval:user-guides:circuits-from-the-lab:cn0264 [29 Jul 2021 05:55] (current) – Hardware Registration Harvey John De Chavez | ||
---|---|---|---|
Line 18: | Line 18: | ||
* [[adi> | * [[adi> | ||
* [[ftp:// | * [[ftp:// | ||
- | * Power Supply | + | * Power Supply |
* 7.5 V or 7.5 V "Wall wart" | * 7.5 V or 7.5 V "Wall wart" | ||
* Spectrum Analyzer | * Spectrum Analyzer | ||
Line 57: | Line 57: | ||
{{ : | {{ : | ||
+ | |||
+ | **Jumper 8** is for the P7 to P0 Output/ | ||
+ | |||
+ | {{ : | ||
+ | \\ | ||
+ | |||
+ | ==== Test setup ==== | ||
+ | {{ : | ||
+ | |||
+ | - Connect the output of the power supply or wall wart to the +7.5V DC connector jumper on the [[ADI> | ||
+ | - Flick the switch next to the “+7.5V DC” connector so that the nearby LED turns on. The [[ADI> | ||
+ | - Connect the Universal Serial Bus (USB) cable from your computer (the computer where ADV Register Control software is installed) to the mini USB connector on the [[ADI> | ||
+ | - Connect video input and output cables | ||
+ | - Launch the evaluation software | ||
---- | ---- | ||
Line 67: | Line 81: | ||
===== Using the Evaluation Software ===== | ===== Using the Evaluation Software ===== | ||
====Main Tab==== | ====Main Tab==== | ||
- | {{ : | + | {{ : |
+ | \\ | ||
+ | \\ | ||
+ | {{ : | ||
| | ||
+ | \\ | ||
+ | |||
+ | ==== Running the System ==== | ||
+ | -Open the ADV Register Control | ||
+ | -When the ADV Register Control opens a window called ADV Register Program Configuration opens, make sure that the “USB Connected” indicator is green | ||
+ | -If indicator doesn' | ||
+ | -Select the proper script according to the model type of your ADV7180. In the case of CN0264 board, ADV7180_ADV7180@_ADV7393-VER.1.0LQFP64.txt shall be selected. | ||
+ | -To program the CN0264 evaluation board press Setting -> Scripts | ||
+ | -Select which script you want to run on the drop down menu. The desired script depends on the analog video inputted to the ADV7180, and the desired analog video output from the video encoder on the evaluation board | ||
\\ | \\ | ||
Line 76: | Line 102: | ||
* [[ftp:// | * [[ftp:// | ||
* [[ADI> | * [[ADI> | ||
- | * [[http:// | + | * [[adi>media/ |
* [[ADI> | * [[ADI> | ||
* [[ADI> | * [[ADI> | ||
Line 85: | Line 111: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | [[http:// | + | [[adi>media/ |
* Schematics | * Schematics | ||
* PCB Layout | * PCB Layout | ||
Line 92: | Line 118: | ||
</ | </ | ||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | </ | ||
//End of Document// | //End of Document// |