This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0264 [14 Nov 2017 08:20] – created Trisha Cabildo | resources:eval:user-guides:circuits-from-the-lab:cn0264 [29 Jul 2021 05:55] (current) – Hardware Registration Harvey John De Chavez | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== CN0264 Evaluation Board Guide ====== | ====== CN0264 Evaluation Board Guide ====== | ||
===== Overview ===== | ===== Overview ===== | ||
- | [[ADI> | + | [[ADI> |
[[ADI> | [[ADI> | ||
Line 11: | Line 11: | ||
The [[adi> | The [[adi> | ||
\\ | \\ | ||
- | {{ : | + | {{ : |
\\ | \\ | ||
---- | ---- | ||
=====Required Equipment===== | =====Required Equipment===== | ||
+ | * [[adi> | ||
+ | * [[ftp:// | ||
+ | * Power Supply (Maximum) | ||
+ | * 7.5 V or 7.5 V "Wall wart" | ||
+ | * Spectrum Analyzer | ||
+ | * Agilent E4440A or equivalent | ||
+ | * PC with the following //Minimum Requirements// | ||
+ | * Windows 7 (32-bit), Windows Vista (32-bit) or Windows XP | ||
+ | * USB interface | ||
+ | |||
+ | ---- | ||
+ | ===== General Setup ===== | ||
+ | ==== Block assignments ==== | ||
+ | {{ : | ||
+ | |||
+ | * The [[adi> | ||
+ | * Terminal block **J1** is RCA jack for the video output | ||
+ | * Terminal block **J2** is the +7.5 V barrel connector for wall wart supply input | ||
+ | * Terminal block **J3** is mini DIN connector for S-video input | ||
+ | * Terminal block **J4** RCA jack for the video input | ||
+ | * Terminal block **J5** is the jumper for power-down mode of ADV7180 | ||
+ | * Terminal block **J6** is mini AB USB port connecting the board to PC | ||
+ | * Terminal block **J7** is the jumper for FIELD pin of ADV7180 | ||
+ | * Terminal block **J8** is the Video Pixel Output Port of ADV7180. Has output configurations for 8-bit or 16-bit mode | ||
+ | * Terminal block **J9** is the RCA jack for CVBS input for ADA4830-2 | ||
+ | * Terminal block **J10** is the jumper for logic high or low in the chip data address pin of serial EEPROM 24LC64 | ||
+ | * Terminal block **J11** is the jumper for power-down/ | ||
+ | * Terminal block **J12** is the jumper for output DC offset enable pin of ADA4417-3 | ||
+ | * Terminal block **J13** is the RCA jack for CVBS input to ADA4433-1, a differential video filter | ||
+ | * Terminal block **J14** is the RCA jack for processed output CVBS signal in ADA4432-1 | ||
+ | * Terminal block **J15** is the RCA jack for positive differential output of ADA4433-1, a differential video filter | ||
+ | * Terminal block **J16** is the RCA jack for negative differential output of ADA4433-1, a differential video filter | ||
+ | * Terminal block **J17** is mini DIN connector for S-video output of DAC1 from ADA4433-1 | ||
+ | * Terminal block **J18** is the jumper for grounding second positive differential input of ADA4830-2 | ||
+ | * Terminal block **J19** is the jumper for grounding second negative differential input of ADA4830-2 | ||
+ | |||
+ | \\ | ||
+ | ==== Jumper settings ==== | ||
+ | See the table in the image below for the jumper settings. Values in red are the default settings for the [[ADI> | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | **Jumper 8** is for the P7 to P0 Output/ | ||
+ | |||
+ | {{ : | ||
+ | \\ | ||
+ | |||
+ | ==== Test setup ==== | ||
+ | {{ : | ||
+ | |||
+ | - Connect the output of the power supply or wall wart to the +7.5V DC connector jumper on the [[ADI> | ||
+ | - Flick the switch next to the “+7.5V DC” connector so that the nearby LED turns on. The [[ADI> | ||
+ | - Connect the Universal Serial Bus (USB) cable from your computer (the computer where ADV Register Control software is installed) to the mini USB connector on the [[ADI> | ||
+ | - Connect video input and output cables | ||
+ | - Launch the evaluation software | ||
+ | |||
+ | ---- | ||
+ | ===== Installing the Evaluation Software ===== | ||
+ | - Extract the file **CN0264_Evaluation_Software.zip** and open the file **setup.bat**.\\ \\ <WRAP left tip round box 60%> | ||
+ | - Click **Next** to view the installation review page\\ \\ {{: | ||
+ | - Click **Next** to start the installation\\ \\ {{: | ||
+ | |||
+ | ---- | ||
+ | ===== Using the Evaluation Software ===== | ||
+ | ====Main Tab==== | ||
+ | {{ : | ||
+ | \\ | ||
+ | \\ | ||
+ | {{ : | ||
+ | | ||
+ | \\ | ||
+ | |||
+ | ==== Running the System ==== | ||
+ | -Open the ADV Register Control | ||
+ | -When the ADV Register Control opens a window called ADV Register Program Configuration opens, make sure that the “USB Connected” indicator is green | ||
+ | -If indicator doesn' | ||
+ | -Select the proper script according to the model type of your ADV7180. In the case of CN0264 board, ADV7180_ADV7180@_ADV7393-VER.1.0LQFP64.txt shall be selected. | ||
+ | -To program the CN0264 evaluation board press Setting -> Scripts | ||
+ | -Select which script you want to run on the drop down menu. The desired script depends on the analog video inputted to the ADV7180, and the desired analog video output from the video encoder on the evaluation board | ||
+ | \\ | ||
+ | |||
+ | ---- | ||
+ | |||
+ | ===== More Information and Useful Links ===== | ||
+ | * [[ftp:// | ||
+ | * [[ADI> | ||
+ | * [[adi> | ||
+ | * [[ADI> | ||
+ | * [[ADI> | ||
+ | * [[ADI> | ||
+ | * [[ADI> | ||
+ | |||
+ | ===== Schematic, PCB Layout, Bill of Materials ===== | ||
+ | |||
+ | <WRAP round 80% download> | ||
+ | [[adi> | ||
+ | * Schematics | ||
+ | * PCB Layout | ||
+ | * Bill of Materials | ||
+ | * PADS project | ||
+ | </ | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | </ | ||
+ | //End of Document// |