This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0254 [06 Dec 2017 03:49] – update Trisha Cabildo | resources:eval:user-guides:circuits-from-the-lab:cn0254 [30 Jul 2021 07:26] (current) – Victor Calinao, Jr | ||
---|---|---|---|
Line 15: | Line 15: | ||
===== Required Equipment ===== | ===== Required Equipment ===== | ||
* [[adi> | * [[adi> | ||
- | * [[http:// | + | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**) |
* [[ftp:// | * [[ftp:// | ||
* DC Power Supply (6 V, 500 mA) | * DC Power Supply (6 V, 500 mA) | ||
Line 26: | Line 26: | ||
==== Block assignments ==== | ==== Block assignments ==== | ||
{{ : | {{ : | ||
- | * The [[http:// | + | * The [[adi>EVAL-CN0254-SDPZ|EVAL-CN0254-SDPZ]] **(CN-0254 Board)** connects to the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector |
- | * The [[http:// | + | * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. |
* Terminal block **CN2** is the +6 V power supply input | * Terminal block **CN2** is the +6 V power supply input | ||
* Terminal block **J2** is for the multiple channels analog input | * Terminal block **J2** is for the multiple channels analog input | ||
Line 34: | Line 34: | ||
==== Test setup ==== | ==== Test setup ==== | ||
{{ : | {{ : | ||
- | - Connect the 120-pin connector on the [[adi> | + | - Connect the 120-pin connector on the [[adi> |
- After setting the dc output supply to 6 V output, turn the supply off | - After setting the dc output supply to 6 V output, turn the supply off | ||
- With power to the supply off, connect 6 V to CN2 | - With power to the supply off, connect 6 V to CN2 | ||
Line 87: | Line 87: | ||
* **Input Range** - Select range of analog signal input | * **Input Range** - Select range of analog signal input | ||
* **Overwrite EEPROM** Checkbox - If selected, precision voltage parameter will be saved into EEPROM after calibration is complete | * **Overwrite EEPROM** Checkbox - If selected, precision voltage parameter will be saved into EEPROM after calibration is complete | ||
- | * **Calibrate** - Start Calibration | + | * **Calibrate** - Start calibration |
- | * **Recover to Default Value** - | + | * **Recover to Default Value** - Recover the original default values of precision voltages of the device from the EEPROM |
- | * **Write Factory Default** - | + | * **Write Factory Default** - Writes precision voltages from calibration to an array in EEPROM and sets them as the factory default values |
- **S/W Version Info** Tab \\ {{ : | - **S/W Version Info** Tab \\ {{ : | ||
* **Flash LED** - Flashes the LED on the SDP controller board | * **Flash LED** - Flashes the LED on the SDP controller board | ||
Line 121: | Line 121: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | [[http:// | + | [[adi>media/ |
* Schematics | * Schematics | ||
* PCB Layout | * PCB Layout | ||
Line 128: | Line 128: | ||
</ | </ | ||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | |||
+ | // End of Document // |