This version is outdated by a newer approved version.This version (18 Sep 2017 04:37) is a draft.
Approvals: 0/1
This is an old revision of the document!
Overview
High-side current monitors are likely to encounter overvoltage conditions from transients or when the monitoring circuits are connected, disconnected, or powered down. This circuit uses the overvoltage protected ADA4096-2 op amp connected as a difference amplifier to monitor the high-side current. The ADA4096-2 has input overvoltage protection, without phase reversal or latch-up, for voltages of 32V higher than and lower than the supply rails.
The circuit is powered by the ADP3336 adjustable low dropout 500 mA linear regulator, which can also be used to supply power to other parts of the system, if desired. Its input voltage can range from 5.2V to 12V when set for a 5V output. To save power, the current sensing circuit can be powered down by removing power to the ADP3336; however, the power source, such as a solar panel, can still operate.
This applies voltage to the inputs of the unpowered ADA4096-2; however, no latch-up or damage occurs for input voltages up to 32V. If slower throughput rates are required, the AD7920 can also be powered down between samples. The AD7920 draws a maximum of 5 μW when powered down and 15 mW when powered up. The ADA4096-2 requires only 120 μA under operational conditions. When operating at 5V, this is only 0.6 mW. The ADP3336 draws only 1 μA in the shutdown mode.
Required Equipment
-
-
-
DC power supply capable of driving 6
V/1 A
DC power supply capable of driving 5
V/2.5 A
2 Ω/12 W load resistor
PC (
minimum: Windows XP) with
USB interface
General Setup
Block Assignments
-
Connect a 6V power supply to the
+6V and
GND pins on the board. If available, a 6
V wall wart can be connected to the barrel connector,
J5, in place of the 6V power supply.
Connect the 5V/2.5 A dc supply to +VIN and GND on J1. Also connect the 2 Ω/12 W load resistor to LOAD and GND on J1.
-
Installing the Evaluation Software
Download and extract the file
CN0241 Evaluation Software and open
setup.exe
NOTE: It is recommended that you install the CN0241 Evaluation Software to the default directory path C:\Program Files (x86)\Analog Devices\CN0241\ and all National Instruments products to C:\Program Files\National Instruments\
Click
Next and accept license agreement.
Click
Next to view the installation review page
Click
Next to start the installation
Upon completion of the installation of the
CN0241 Evaluation Software, the installer for the
ADI SDP Drivers will execute.
NOTE: It is recommended that you close all other applications before clicking “Next”. This will make it possible to update relevant system files without having to reboot your computer.
Click
Next to set the installation location for the
SDP Drivers
It is recommended that you install the drivers to the default directory path
C:\Program Files\Analog Devices\SDP\Drivers
Click
Next to install the
SDP Drivers. When prompted by Windows Security, just press
Install
Click
Finish to complete the installation
Using the Evaluation Software
Main Window
Title Bar
Menu Bar
Select SDP connector - Selects which 120-pin connection of the SDP-B Board to use.
Sample Size
Sample Data Button - Starts the acquisition of measurement data.
Save Data Button - Saves the acquired measurement data.
Selection Tab
Sample Data Tab
Shows the acquired measurement data in terms of ADC codes with respect to the samples.
By right-clicking within the area, more functions can be viewed. Graph palette can be hidden by deselecting it and also other items can be added such as plot legend, scale legend, etc.
Histogram Tab
Shows the acquired measurement data in terms of Number of counts with respect to the ADC codes
The same as the previous tab, by right-clicking within the area, more functions can be viewed. Other items can be added such as plot legend, scale legend, etc.
Configure Tab
AD7920 Mode - Can choose between two modes:
Read Firmware - Reads the firmware of CN0241 Evaluation Board
Flash LED - Flashes the LED on the SDP controller board
Quit Button
Running the System
Apply power to the 6V supply (or wall wart) connected to the CN0241 evaluation board.
Connect
USB cable from PC to the
USB miniconnector on the SDP-B board.
Launch CN0241 Evaluation Software from the default installation location.
Click “Connect” to start communication between SDP-B and CN0241.
Upon successful connection, select SDP connector used, either connector A or connector B.
Set the desired number of samples.
Turn the 5
V/2.5 A dc supply on when data is ready to be acquired.
Adjust the voltage output accordingly to output the amount of current needed to be measured
Click “Sample Data” to start acquisition of data.
Schematic, PCB Layout, Bill of Materials