Wiki

This version is outdated by a newer approved version.DiffThis version (27 Oct 2017 08:31) is a draft.
Approvals: 0/1

This is an old revision of the document!


CN0218 Evaluation Board Guide

Overview

CN0218 is a circuit that monitors current in systems with high positive common-mode dc voltages of up to +500 V with less than 0.2% error. The load current passes through a shunt resistor, which is external to the circuit. The circuit is designed for a full-scale shunt voltage of 500 mV at maximum load current Imax.

The AD8212 is a high common-mode voltage, current shunt monitor. It accurately amplifies a small differential input voltage in the presence of large common-mode voltages up to 65 V (>500 V with an external PNP transistor). The AD8605 is a single rail-to-rail input and output, single-supply amplifier. It features very low offset voltage, low input voltage and current noise, and wide signal bandwidth.

The AD7171 is a very low power, 16-bit, analog-to-digital converter (ADC). It contains a precision, 16-bit, Σ-Δ ADC and an on-chip oscillator. The measurement result from AD7171 is provided as a digital code utilizing a simple 2-wire, SPI-compatible serial interface.

The ADuM5402 is a quad channel isolator that provides galvanic isolation for the circuit. This is not only for protection but to isolate the downstream circuitry from the high common-mode voltage. In addition to isolating the output data, the digital isolator can also supply isolated +3.3 V for the circuit.

The ADR381 is precision 2.500 V band gap voltage reference featuring high accuracy, high stability, and low power consumption in a tiny footprint. It is a micropower, low dropout voltage (LDV) device that provides a stable output voltage from supplies as low as 300 mV above the output voltage.

The EVAL-CN0218-SDPZ Board connects to ADI’s System Demonstration Platform (SDP) and is powered by a +6 V supply or +6 V “wall wart”.


Required Equipment


General Setup

Block assignments



High voltage! This circuit may contain lethal voltages. Do not operate, evaluate, or test this circuit, or board assembly, unless you are a trained professional, who is qualified to handle high voltage circuitry. Before applying power, you must be familiar with the circuitry and all required precautions for working with high voltage circuits.


Do not connect the USB cable to the Mini-USB connector on the SDP board before turning on the dc power supply for the EVAL-CN0218-SDPZ.


Installing the Evaluation Software

  1. Extract the file CN0218_Evaluation_Software.zip and open the file setup.exe.

    NOTE: It is recommended that you install the CN0218 Evaluation Software to the default directory path C:\Program Files (x86)\Analog Devices\CN0218\ and all National Instruments products to C:\Program Files\National Instruments\

  2. Click Next to view the installation review page



  3. Click Next to start the installation



  4. Upon completion of the installation of the CN-0188 Evaluation Software, the installer for the ADI SDP Drivers will execute.

    NOTE: It is recommended that you close all other applications before clicking “Next”. This will make it possible to update relevant system files without having to reboot your computer.





  5. Press “Next” to set the installation location for the SDP Drivers.

    It is recommended that you install the drivers to the default directory path
    C:\Program Files\Analog Devices\SDP\Drivers





  6. Press “Install” to install the SDP Drivers and complete the installation of all software. Click “Finish” when done.


Using the Evaluation Software

Test Setup Tab




Schematic, PCB Layout, Bill of Materials

EVAL-CN0218-SDPZ Design & Integration Files

  • Schematics
  • PCB Layout
  • Bill of Materials
  • PADS project

End of Document

resources/eval/user-guides/circuits-from-the-lab/cn0218.1509085916.txt.gz · Last modified: 27 Oct 2017 08:31 by Trisha Cabildo