This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0218 [28 Nov 2017 02:36] – update eval software Trisha Cabildo | resources:eval:user-guides:circuits-from-the-lab:cn0218 [30 Jul 2021 07:22] (current) – Victor Calinao, Jr | ||
---|---|---|---|
Line 15: | Line 15: | ||
===== Required Equipment ===== | ===== Required Equipment ===== | ||
* [[adi> | * [[adi> | ||
- | * [[http:// | + | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**) |
* [[ftp:// | * [[ftp:// | ||
* Power Supply | * Power Supply | ||
Line 29: | Line 29: | ||
==== Block assignments ==== | ==== Block assignments ==== | ||
{{ : | {{ : | ||
- | * The [[http:// | + | * The [[adi>EVAL-CN0150-SDPZ|EVAL-CN0150-SDPZ]] **(CN-0150 Board)** connects to the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector |
- | * The [[http:// | + | * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. |
* Terminal block **J1** is the SDP connector | * Terminal block **J1** is the SDP connector | ||
* Terminal block **J2** is the +6 V barrel connector for wall wart supply input | * Terminal block **J2** is the +6 V barrel connector for wall wart supply input | ||
Line 42: | Line 42: | ||
{{ : | {{ : | ||
- | - Connect the 120-pin connector on the [[adi> | + | - Connect the 120-pin connector on the [[adi> |
- Connect a shunt resistor across the input terminals with a load to ground as indicated in figure above | - Connect a shunt resistor across the input terminals with a load to ground as indicated in figure above | ||
- With power to the supply off, connect a +6 V power supply to the pins marked “+6V” and “GND” on the board | - With power to the supply off, connect a +6 V power supply to the pins marked “+6V” and “GND” on the board | ||
Line 71: | Line 71: | ||
- **Connect** Button - Starts the connection between the [[ADI> | - **Connect** Button - Starts the connection between the [[ADI> | ||
- **Reset and Disconnect** - Resets the board and ends the connection between the [[ADI> | - **Reset and Disconnect** - Resets the board and ends the connection between the [[ADI> | ||
- | - **Stop** Button - Stop the program of CN0218 | + | - **Stop** Button - Stop collecting data from the CN0218 Board |
- **Test Setup** Tab - Shows the acquired measurement data in terms of shunt voltage with respect to the samples\\ {{ : | - **Test Setup** Tab - Shows the acquired measurement data in terms of shunt voltage with respect to the samples\\ {{ : | ||
* **Shunt Voltage** - Shunt voltage measurement output from ADC | * **Shunt Voltage** - Shunt voltage measurement output from ADC | ||
* **Click to Start Sampling** - Starts acquisition of measurement data | * **Click to Start Sampling** - Starts acquisition of measurement data | ||
- | * **Clear Data** - Clears the current measurement | + | * **Clear Data** - Clear all data collected from the chart history |
* **Save Data to File** - Save measurement data to file | * **Save Data to File** - Save measurement data to file | ||
- **Configure** Tab\\ {{ : | - **Configure** Tab\\ {{ : | ||
Line 83: | Line 83: | ||
\\ | \\ | ||
+ | ==== Running the System ==== | ||
+ | -Open the CN0218.exe application from the default installation location | ||
+ | -Click the Connect Button | ||
+ | -Upon successful connection, start and control data acquisition through the data acquisition control buttons | ||
+ | -Output data will be shown in the graph. Edit graph through plot options and check boxes provided | ||
+ | -Click Disconnect if finished | ||
+ | -Click Quit to exit the program | ||
---- | ---- | ||
Line 88: | Line 95: | ||
* [[ftp:// | * [[ftp:// | ||
* [[ADI> | * [[ADI> | ||
- | * [[http:// | + | * [[adi>media/ |
* [[ADI> | * [[ADI> | ||
* [[ADI> | * [[ADI> | ||
Line 98: | Line 105: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | [[http:// | + | [[adi>media/ |
* Schematics | * Schematics | ||
* PCB Layout | * PCB Layout | ||
Line 104: | Line 111: | ||
* PADS project | * PADS project | ||
</ | </ | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
//End of Document// | //End of Document// | ||