This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0218 [04 Dec 2017 11:03] – update Trisha Cabildo | resources:eval:user-guides:circuits-from-the-lab:cn0218 [30 Jul 2021 07:22] (current) – Victor Calinao, Jr | ||
---|---|---|---|
Line 15: | Line 15: | ||
===== Required Equipment ===== | ===== Required Equipment ===== | ||
* [[adi> | * [[adi> | ||
- | * [[http:// | + | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**) |
* [[ftp:// | * [[ftp:// | ||
* Power Supply | * Power Supply | ||
Line 29: | Line 29: | ||
==== Block assignments ==== | ==== Block assignments ==== | ||
{{ : | {{ : | ||
- | * The [[http:// | + | * The [[adi>EVAL-CN0150-SDPZ|EVAL-CN0150-SDPZ]] **(CN-0150 Board)** connects to the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector |
- | * The [[http:// | + | * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. |
* Terminal block **J1** is the SDP connector | * Terminal block **J1** is the SDP connector | ||
* Terminal block **J2** is the +6 V barrel connector for wall wart supply input | * Terminal block **J2** is the +6 V barrel connector for wall wart supply input | ||
Line 42: | Line 42: | ||
{{ : | {{ : | ||
- | - Connect the 120-pin connector on the [[adi> | + | - Connect the 120-pin connector on the [[adi> |
- Connect a shunt resistor across the input terminals with a load to ground as indicated in figure above | - Connect a shunt resistor across the input terminals with a load to ground as indicated in figure above | ||
- With power to the supply off, connect a +6 V power supply to the pins marked “+6V” and “GND” on the board | - With power to the supply off, connect a +6 V power supply to the pins marked “+6V” and “GND” on the board | ||
Line 95: | Line 95: | ||
* [[ftp:// | * [[ftp:// | ||
* [[ADI> | * [[ADI> | ||
- | * [[http:// | + | * [[adi>media/ |
* [[ADI> | * [[ADI> | ||
* [[ADI> | * [[ADI> | ||
Line 105: | Line 105: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | [[http:// | + | [[adi>media/ |
* Schematics | * Schematics | ||
* PCB Layout | * PCB Layout | ||
Line 111: | Line 111: | ||
* PADS project | * PADS project | ||
</ | </ | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
//End of Document// | //End of Document// | ||