Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0218 [03 Nov 2017 08:37] – update Trisha Cabildoresources:eval:user-guides:circuits-from-the-lab:cn0218 [30 Jul 2021 07:22] (current) Victor Calinao, Jr
Line 15: Line 15:
 ===== Required Equipment ===== ===== Required Equipment =====
   * [[adi>EVAL-CN0218-SDPZ|EVAL-CN0218-SDPZ Evaluation Board]]   * [[adi>EVAL-CN0218-SDPZ|EVAL-CN0218-SDPZ Evaluation Board]]
-  * [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**)+  * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**)
   * [[ftp://ftp.analog.com/pub/cftl/CN0218/|CN0218 Evaluation Software]]   * [[ftp://ftp.analog.com/pub/cftl/CN0218/|CN0218 Evaluation Software]]
   * Power Supply   * Power Supply
Line 29: Line 29:
 ==== Block assignments ==== ==== Block assignments ====
 {{ :resources:eval:user-guides:circuits-from-the-lab:cn0218:8.png?nolink&550 |}}\\ {{ :resources:eval:user-guides:circuits-from-the-lab:cn0218:8.png?nolink&550 |}}\\
-  * The [[http://www.analog.com/EVAL-CN0150-SDPZ|EVAL-CN0150-SDPZ]] **(CN-0150 Board)** connects to the [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector +  * The [[adi>EVAL-CN0150-SDPZ|EVAL-CN0150-SDPZ]] **(CN-0150 Board)** connects to the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector 
-  * The [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable.+  * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable.
   * Terminal block **J1** is the SDP connector   * Terminal block **J1** is the SDP connector
   * Terminal block **J2** is the +6 V barrel connector for wall wart supply input   * Terminal block **J2** is the +6 V barrel connector for wall wart supply input
Line 42: Line 42:
 {{ :resources:eval:user-guides:circuits-from-the-lab:cn0218:9.png?nolink&600 |}}\\ {{ :resources:eval:user-guides:circuits-from-the-lab:cn0218:9.png?nolink&600 |}}\\
  
-  - Connect the 120-pin connector on the [[adi>EVAL-CN0218-SDPZ|EVAL-CN0218-SDPZ Evaluation Board]] to the connector marked “CON A” on the [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] evaluation (SDP) board+  - Connect the 120-pin connector on the [[adi>EVAL-CN0218-SDPZ|EVAL-CN0218-SDPZ Evaluation Board]] to the connector marked “CON A” on the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] evaluation (SDP) board
   - Connect a shunt resistor across the input terminals with a load to ground as indicated in figure above   - Connect a shunt resistor across the input terminals with a load to ground as indicated in figure above
   - With power to the supply off, connect a +6 V power supply to the pins marked “+6V” and “GND” on the board   - With power to the supply off, connect a +6 V power supply to the pins marked “+6V” and “GND” on the board
Line 61: Line 61:
   - Click **Next** to view the installation review page\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0218:2.png?nolink&500|}}\\ \\   - Click **Next** to view the installation review page\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0218:2.png?nolink&500|}}\\ \\
   - Click **Next** to start the installation\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0218:3.png?nolink&500|}}\\ \\   - Click **Next** to start the installation\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0218:3.png?nolink&500|}}\\ \\
-  - Upon completion of the installation of the **CN-0188 Evaluation Software**, the installer for the **ADI SDP Drivers** will execute.\\ \\ <WRAP left tip round box 60%>**NOTE:** It is recommended that you close all other applications before clicking **“Next”**.  This will make it possible to update relevant system files without having to reboot your computer.</WRAP>\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0218:4.png?nolink&500|}}\\ \\+  - Upon completion of the installation of the **CN-0218 Evaluation Software**, the installer for the **ADI SDP Drivers** will execute.\\ \\ <WRAP left tip round box 60%>**NOTE:** It is recommended that you close all other applications before clicking **“Next”**.  This will make it possible to update relevant system files without having to reboot your computer.</WRAP>\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0218:4.png?nolink&500|}}\\ \\
   - Press **“Next”** to set the installation location for the **SDP Drivers**.\\ \\ <WRAP left round tip 50%>It is recommended that you install the drivers to the default directory path \\ **C:\Program Files\Analog Devices\SDP\Drivers**</WRAP>\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0218:5.png?nolink&500|}}\\ \\   - Press **“Next”** to set the installation location for the **SDP Drivers**.\\ \\ <WRAP left round tip 50%>It is recommended that you install the drivers to the default directory path \\ **C:\Program Files\Analog Devices\SDP\Drivers**</WRAP>\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0218:5.png?nolink&500|}}\\ \\
   - Press **“Install”** to install the **SDP Drivers** and complete the installation of all software.  Click **"Finish"** when done.\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0218:6.png?nolink&500|}}   - Press **“Install”** to install the **SDP Drivers** and complete the installation of all software.  Click **"Finish"** when done.\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0218:6.png?nolink&500|}}
Line 67: Line 67:
 ---- ----
 ===== Using the Evaluation Software ===== ===== Using the Evaluation Software =====
-====Test Setup Tab==== +==== Main Window ==== 
-{{ :resources:eval:user-guides:circuits-from-the-lab:cn0218:7.png?nolink&650 |}}\\ +{{ :resources:eval:user-guides:circuits-from-the-lab:cn0218:17.png?nolink&700 |}} 
-  +  - **Connect** Button - Starts the connection between the [[ADI>CN0218|CN0218 Evaluation Board]] and [[ADI>EVAL-SDP-CB1Z|SDP-B Controller Board]]. 
 +  - **Reset and Disconnect** - Resets the board and ends the connection between the [[ADI>CN0218|CN0218 Evaluation Board]] and [[ADI>EVAL-SDP-CB1Z|SDP-B Controller Board]] 
 +  - **Stop** Button - Stop collecting data from the CN0218 Board 
 +  - **Test Setup** Tab - Shows the acquired measurement data in terms of shunt voltage with respect to the samples\\ {{ :resources:eval:user-guides:circuits-from-the-lab:cn0218:14.png?nolink&600 |}} 
 +      * **Shunt Voltage** - Shunt voltage measurement output from ADC 
 +      * **Click to Start Sampling** - Starts acquisition of measurement data 
 +      * **Clear Data** - Clear all data collected from the chart history  
 +      * **Save Data to File** - Save measurement data to file 
 +  - **Configure** Tab\\ {{ :resources:eval:user-guides:circuits-from-the-lab:cn0218:15.png?nolink&600 |}} 
 +      * **Flash LED** - Flashes the LED on the SDP controller board 
 +      * **Read Firmware** - Reads the firmware of CN0218 Evaluation Board  
 +  - **Plot** Options -  Edit plot display and options like interpolation and color of output waveform \\ {{ :resources:eval:user-guides:circuits-from-the-lab:cn0218:18.png?nolink&600 |}}
 \\ \\
  
 +==== Running the System ====
 +  -Open the CN0218.exe application from the default installation location
 +  -Click the Connect Button
 +  -Upon successful connection, start and control data acquisition through the data acquisition control buttons
 +  -Output data will be shown in the graph. Edit graph through plot options and check boxes provided
 +  -Click Disconnect if finished
 +  -Click Quit to exit the program
 ---- ----
  
Line 77: Line 95:
   * [[ftp://ftp.analog.com/pub/cftl/CN0218/|CN0218 Evaluation Software]]   * [[ftp://ftp.analog.com/pub/cftl/CN0218/|CN0218 Evaluation Software]]
   * [[ADI>CN0218|CN0218 Circuit Note Page]]   * [[ADI>CN0218|CN0218 Circuit Note Page]]
-  * [[http://www.analog.com/media/en/reference-design-documentation/design-integration-files/CN0218-DesignSupport.zip|CN0218 Design Support Package]]+  * [[adi>media/en/reference-design-documentation/design-integration-files/CN0218-DesignSupport.zip|CN0218 Design Support Package]]
   * [[ADI>AD8212|AD8212 Product Page]]   * [[ADI>AD8212|AD8212 Product Page]]
   * [[ADI>AD7171|AD7171 Product Page]]   * [[ADI>AD7171|AD7171 Product Page]]
Line 87: Line 105:
  
 <WRAP round 80% download> <WRAP round 80% download>
-[[http://www.analog.com/media/en/reference-design-documentation/design-integration-files/CN0218-DesignSupport.zip|EVAL-CN0218-SDPZ Design & Integration Files]]+[[adi>media/en/reference-design-documentation/design-integration-files/CN0218-DesignSupport.zip|EVAL-CN0218-SDPZ Design & Integration Files]]
   * Schematics    * Schematics 
   * PCB Layout    * PCB Layout 
Line 93: Line 111:
   * PADS project   * PADS project
 </WRAP> </WRAP>
 +
 +=====Registration===== 
 +<WRAP round tip 80% >
 +Receive software update notifications, documentation updates, view the latest videos, and more when you register your hardware.  [[reg>EVAL-CN0218-SDPZ?&v=Rev A|Register]] to receive all these great benefits and more!</WRAP>
  
 //End of Document// //End of Document//
  
resources/eval/user-guides/circuits-from-the-lab/cn0218.txt · Last modified: 30 Jul 2021 07:22 by Victor Calinao, Jr